There are two ways to update the Trusted-firmware(TF) and U-boot.
The first way is using the built-in commands of the Flashwriter-tool to download TF and U-boot images (.srec format only) to RAM and then write them to the bootable devices (eMMC or QSPI-Flash). It works using the SCIF Download Mode boot mode of the device. This way is introduced in the Startup Guide inside BSP release's documents, which will not be described in detail in this page. The advantage of this method is that it can be used for any board, especially for the new boards with empty bootable devices. But there are disadvantage for this method. For example, it's very slow because when using SCIF Download Mode, data is transferred via UART port at 115200bps. And, the user must manually input some data or select some files for each board during updating process.
The second method will be described in detail in this page. This method is updating the TF and U-boot images (.bin, raw binary format only) under Linux. It's accomplished using very common commands such as dd, flash_eraseall, cat and so on. So it's very fast and the commands can be written into a shell script which can be run automatically after boot into Linux. But the disadvantage is that this method cannot work with new boards with an empty bootable device. For these kinds of boards, you must use the first method described above.
Users do not want to use the first method only because of the disadvantages of this method (speed or programming). They prefer to use the two methods at the same time. RZ/G series MPUs support the use of QSPI flash and eMMC as boot devices. Typically the eMMC is used as the main boot device for products. Product developers can make a small board with only a QSPI flash mounted on it. This small board can be plugged into the main product board. Using this type of temporary boot device is similar to how a PC can boot from a bootable USB flash drive and then be used to install used to install the whole OS system to an PC's hard disk.
Typical usage steps:
After step 8, the QSPI flash board is ready. Developers can also update an empty QSPI flash boards after boot into Linux from eMMC boot mode. So developers only need to use the first method to update an empty QSPI flash board once, then every board can be updated under Linux.
After booting into Linux, you should prepare the binary format of TF and U-boot. We cannot use the srec format because the common Linux based commands cannot interpret or recognize s-record format unlike the built-in commands inside Flashwriter. We only need to know the offset inside the boot device to store the binary file and then write the binary from the offset. These offsets are just the requirements of the Boot ROM or TF.
From the release note document, we can get the offset information(the 'Address to save to ROM' column).
...
Image Added
The 0x00000 and 0x1D200(=512x233) are the offsets from the QSPI flash memory base. We can make an image first and then write the image into /dev/mtd0.
dd if=/dev/zero of=boot.img bs=1024 count=1024
dd if=bl2_bp.bin of=boot.img conv=notrunc
dd if=fip-smarc-rzg2l.bin of=boot.img conv=notrunc bs=512 seek=233
flashcp -v boot.img /dev/mtd0
Note:
The u-boot environment variables are stored into eMMC Boot1 partition(the 2nd Boot partition) by default. If you want to store them into the QSPI Flash, please refer to this link: RZ-G/RZG uboot#Use SPI Flash for Env Variables.
From the Release Note document include in the BSP, we know that the TF and U-boot are written into Boot0 area of eMMC. The sector offsets are 1 and 256 with sector size 512. The EXT_CSD registers are also needed to be setup according to the document.
mmc bootpart enable 1 0 /dev/mmcblk0 # enable the first boot-area 0 for boot, no ack
mmc bootbus set single_backward x1 x8 /dev/mmcblk0 # setup the boot bus config
echo 0 > /sys/block/mmcblk0boot0/force_ro # disable the soft write-protect based on Linux, reset after reboot
dd if=bl2_bp.bin of=/dev/mmcblk0boot0 bs=512 skip=0 seek=1
dd if=fip-smarc-rzg2l.bin of=/dev/mmcblk0boot0 bs=512 skip=0 seek=256
The basic scheme for these MPU types is the same as RZ/G2L. The differences are that the TF may contain several binary files with different offsets or boot areas.
Table of Contents |
---|