...
- SW1003: change bit 4 to OFF to enable JTAG
- SW305: change to (2-3) side
- SW2405: change to (1-2) side
Tigrad Tigard Switch Setting
If you are using a TigradTigard, set the TARGET switch to 1v8
...
- To debug with J-Link, the following script is available: share/openocd/scripts/interface/jlink.cfg
- To debug with TigradTigard, the following script is available: share/openocd/scripts/interface/ftdi/tigard.cfg
...
- The Device configuration file for the RZ family is share/openocd/scripts/target/renesas_rz.cfg
- Note: In the Official OpenOCD repository, the file name is renesas_rz_g2.cfg. However, in the patches you downloaded and ran, we renamed it to renesas_rz.cfg. We plan to mainline this change back into the official openocd repository eventuallyÂ
...
Example to run OpenOCD and attach to a RZ/G2L device using a Tigrad Tigard JTAG adapter:
$ cd installdir
$ sudo bin/openocd -f share/openocd/scripts/interface/ftdi/tigard.cfg -c "set SOC G2L" -f share/openocd/scripts/target/renesas_rz.cfg
...