Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

.Links
📦 RZ/G2 Linux Package (Common for all MPU    )
ZIP file containing Yocto BSP and all documentation
  • Yocto Recipe
    This is the actual BSP provided in a Yocto build package
  • Release Note for Linux Package
    Build instructions, start with this document
  • Reference Boards Linux Start-up Guide
    How to program the boot loaders into SPI flash
  • BSP Component list
    List of each package and version included in the default BSP build

RZ/G2 (all)
💾 Download Page


RZ/V2L, RZ/V2MA, RZ/V2M

💾 Download Page


RZ/V2H
Contact Renesas

🎨 Graphics (PowerVR) and 🎦 Video Codec Libraries
  • For devices RZ/G2H, RZ/G2M, RZ/G2N, RZ/G2E
  • The "Evaluation Version" can be downloaded immediately, but has a 2 hour timeout after every board boot.
  • The "Unrestricted Version" request link is at the at the bottom of the download page (see Note1 below)

RZ/G2H, RZ/G2M, RZ/G2N, RZ/G2E

💾Multimedia Download Page

🎨 Graphics (Mali) Libraries
  • For devices RZ/G2L, RZ/G2LC, RZ/V2L
  • The "Evaluation Version" can be downloaded immediately, but has a 2 hour timeout after every board boot.
  • The "Unrestricted Version" request link is at the at the bottom of the download page (see Note1 below)

RZ/G2L, RZ/G2LC, RZ/G2UL
💾Download Page


RZ/V2L
💾 Download Page

🎦 Video Codec Libraries
  • For devices RZ/G2L and RZ/V2L
RZ/G2L
💾Download Page

RZ/V2L
💾 Download Page
🌐 HTML5 Browser (Gecko/Firefox)
  • For devices some devices
💾 Download Page
📄 BSP Manual Set
Detailed information about Device Drivers and Device Tree Settings
📄 RZ/G2H, RZ/G2M, RZ/G2N, and RZ/G2E (link)

📄 RZ/G2L,RZ/G2LC, RZ/G2UL, RZ/V2L (link)

...

Fix glibc Fetch Error During BSP Build

A file was Files were removed from the Debian server which causes a build error when building the Yocto BSP .

Below are patches in order to fix those issue.

v3.0.6.

  • glibc_2.28-10+deb10u2.debian.tar.xz   (Removed from Server in May, 2024)
  • glibc_2.28-10+deb10u3.debian.tar.xz    (Removed form Server in July 2024)

This effects Patch BSP v3.0.6 and , v3.0.6-update1, v3.0.6-update2

Below are instructions to download and apply patches to fix those issues.Change from deb10u2 to deb10u3, then to deb10u4

cd meta-renesas
# Change deb10u2 to dev10u3
wget https://github.com/renesas-rz/meta-renesas/commit/a56169f6642d.patch
git am a56169f6642d.patch
wget https://github.com/renesas-rz/meta-renesas/commit/6c11ae542069-p1 -i a56169f6642d.patch
git
# am 6c11ae542069.patch

Patch BSP v3.0.6-update2

Change from deb10u3 to deb10u4

Change deb10u3 to dev10u4cd meta-renesas
wget https://github.com/renesas-rz/meta-renesas/commit/6c11ae542069.patch
git ampatch -p1 -i 6c11ae542069.patch


Linux Kernel 4.19 BSP

...