Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

Connect the 9-pin J-Link connector:

Image RemovedImage Added

GR-Mango and J-Link connection

Modify the debug configuration as described for GR-PEACH, but with a different device name for GR-MANGO:

Target Device: R7S921058

Image RemovedImage Added

e²studio debug configuration for GR-MANGO plus J-Link

...

Plug the RZ GR board into the PC.

GR-MANGO

image 2021-08-20 145958.pngImage Removed

Image Added

GR-PEACH

Image Removed

Image Added

MBED USB Debug Port

GR-LYCHEE

Image Removed

Image Added

MBED USB Debug connector

Open the Windows OS Device Manager. You should see the device here.

image 2021-08-20 145402.pngImage RemovedImage Added