Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

Fix glibc Fetch Error During BSP Build

  • Affected BSP: All

Files were removed from the the Debian server which causes a build error when building the BSP v3.0.6.

...

cd meta-renesas
# Change deb10u2 to dev10u3
wget https://github.com/renesas-rz/meta-renesas/commit/a56169f6642d.patch
patch -p1 -i a56169f6642d.patch

# Change deb10u3 to dev10u4
wget https://github.com/renesas-rz/meta-renesas/commit/6c11ae542069.patch
patch -p1 -i 6c11ae542069.patch


RZ/G2 gstreamer1.0-omx-1.16.3-r0 do_fetch Error

  • Affected BSP: RZ/G2H, RZ/G2M, RZ/G2N, RZ/G2E

The Multimedia Package for RZ/G2 on renesas.com is V1.0.2

When building, the follow error will occur.

ERROR: gstreamer1.0-omx-1.16.3-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://anongit.freedesktop.org/gstreamer/common;destsuffix=git/common;name=common')

The reason is that the server name has change from anongit.freedesktop.org to gitlab.freedesktop.org

The easiest way to fix this issue is to run the command below from the base of your BSP directory.

sed -i 's/anongit/gitlab/' meta-rz-features/meta-rz-codecs/recipes-multimedia/gstreamer/gstreamer1.0-omx_1.16.3.bbappend


Linux Kernel 4.19 BSP

...