RZ/A Series 32-bit MPU
Introduction
Image Modified
This page is for the Renesas RZ/A family of embedded SoCs. The main goal is to make the information about RZ/A SoCs friendly, easy to access for embedded developers.
The links below can be used to get familiar with Renesas RZ/A SoC
Boards
- Here is the list of available Renesas Evaluation Boards (bottom of page).
- The board pages below contain instructions for downloading and building the BSP as well as other useful information about the boards.
RZ/A3
...
RZ/A2M
...
RZ/A1
...
Official Software and Documentation
These are the currently supported Software packages for the RZA1 and RZA2M. The
Renesas Supported Development Environments
- Renesas e2studio
- RZA1 Smart Configurator
- NOTE: The RZA1 is not supported on the Smart Configurator found in the Renesas e2studio IDE.
- This Smart Conjugator is a standalone application
- Hardware Pin Configuration is supported
- Code Generation not supported
RZA GUI Platforms
- Microsoft Azure GUIX demos
- TES Guiliani demos Support Page
- Crank contact Crank for RZA demos
- MicroEJ contact MicroEJ for RZA Java demos
- Tara Embedded Wizard contact Tara for RZA demos
RZA Bootloaders
Below are links to Source code for the RZ/A bootloaders and firmware update. These are reference code that was designed for the Renesas RZ/A EVKs. Included below are links to porting documentation.
RZA1
- RZ/A1 Bootloader
- RZA firmware update
- The RZA1 does not have Firmware Update reference code.
- Refer to the RZA2M Firmware Update for Serial Flash Driver to port to the RZA1.
RZA2M
- RZ/A2M Group Example of booting from OctaFlash™ using SPI multi I/O bus controller doc, Source Code
- RZA2M Firmware update ( rza2m_fw_update_sample_freertos_gcc.zip )
Articles and Whitepapers
Topics
FAQ