Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

Finally you can use Yocto to generate the root file system including all the bits and bobs you need to run your custom application...


Individual Software Sections

Flash Writer

Arm Trusted Firmware

Trusted Firmware-A

u-boot

Linux Kernel

Yocto

Ubuntu

OpenWRT

Debian

Yocto

Ubuntu

OpenWRT

Debian

Software Update


Memory Map

Changing Console Port

You can make use of the following changes to change console port from SCIF0 to SCIF2 in RZ/G2L-LC and RZ/V2L (Not applicable for RZ/G2UL). Please note that it NOT RECOMMENDED by Renesas to do so and is described here only for experimental purpose.

...