Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

  • DA14585/DA14586/DA14531/DA14531-01/DA14530/DA14531MOD
  • DA14592


Image Modified

SmartBond™ DA14592 Bluetooth® Low Energy 5.2 SoC Development Kit Pro


The daughterboard is mounted with a WLCSP-packaged DA14592Image Modified

The daughterboard is mounted with a WLCSP-packaged DA14592


The daughterboard is mounted with an FCQFN-packaged DA14592Image Modified

The daughterboard is mounted with an FCQFN-packaged DA14592


Image Modified

DA14531 SmartBond TINY™ Development Kit Pro


DA14531 PRO-daughterboard (PRO-DB) FCGQFN24Image Modified

DA14531 PRO-daughterboard (PRO-DB) FCGQFN24


DA14531-01 PRO-daughterboard (PRO-DB) FCGQFN24Image Modified

DA14531-01 PRO-daughterboard (PRO-DB) FCGQFN24


DA14530 PRO-daughterboard (PRO-DB) FCGQFN24Image Modified

DA14530 PRO-daughterboard (PRO-DB) FCGQFN24


DA14585 PRO-daughterboard (PRO-DB) FCGQFN40Image Modified

DA14585 PRO-daughterboard (PRO-DB) FCGQFN40


DA14586 PRO-daughterboard (PRO-DB) FCGQFN40Image Modified

DA14586 PRO-daughterboard (PRO-DB) FCGQFN40


Image Modified

DA14531 Smartbond TINY™ MODULE Daughter Board



Image Modified

DA14531 SmartBond TINY™ USB Development Kit






 

 


Datasheets

DA14592

DA14531

...

Next to the software examples the user can find useful information in a selection of on-line tutorials. Below is a list of Tutorials with short description:

DA14592

TitleDescription
DA14592 Getting startedThis tutorial is an introduction into SDK10. It explains how to implement basic functionality in the embedded firmware
Software Platform Reference ManualThis document explains deeply the SDK
Tutorial BLE Custom ServiceTutorial explaining what is a custom GATT profile and how to create one
Tutorial Advertising ConceptsTutorial describing how to create a BLE advertiser
Tutorial Starting a ProjectExplains how to start your first project on DA14592 and e2 Studio

DA14531, DA14585/DA14586

TitleDescription
SDK6 Getting startedThis tutorial is an introduction into SDK6. It explains how to implement basic functionality in the embedded firmware
SDK6 peripheral driversThis document provides info about the available low level drivers in the SDK and how to use them
Booting from OTP and SerialThis document explains the various boot options from the external interface
BLE advertiserTutorial describing how to create a BLE advertiser
Create a custom GATT ProfileTutorial explaining what is a custom GATT profile and how to create one
BLE Sleep modesExplains how to create a device with lowest possible power consumption
BLE securityThe tutorial gives basic understanding of BLE security and how to use this on SDK6
Flash selector GuideAn overview of Flash devices that has been verified for DA145xx and SDK6
Tutorial SW debuggingTips and tricks on the various debugging techniques

DA1469x

TitleDescription
Starting a projectThe tutorial explains how to start your own SDK10 project
Using the Adapters in SDK10Using the I2C the Adapter concept is explained as used in SDK10
Booting from Serial interfacesThis document explains the various boot options from the UART or QSPI Flash
BLE advertiserTutorial describing how to create a BLE advertiser
Flash Driver CreationHow to develop a new custom QSPI driver for Flash or RAM
Flash Adaptor for Data StorageHow to implement Non-Voltatile data storage using the available adapter
How to use images bigger than 512Document explaining how to configure the SDK to run images larger than the default 512kB
Power managementTutorial explaining how to define hardware and software set-up for power consumption measurements
Secure Boot MechanismThe document explains how to use the feature of secure boot in the project

Renesas SmartBond Mobile Applications

...