If you encounter any issues after the upgrade, please open a support request TICKET.🙌
Getting Started with the RL78 Family Development Environment
The above webpage introduces the tools required for development, recommended kits, and information on downloading products for new users of the RL78 family development environment.
Development environment pre-installation: (choose either one)
Board:
Emulator:
In the CS+ development environment, Blinky's sample code is not provided. It is necessary to create the project manually. The following steps can be used as a guide.
Create a new project via File->New->Create New Project….
Select “R7F100GLGxFA” and provide an appropriate name for the project. Then click “Create”.
Open Smart Configurator by double-clicking “Smart Configurator (Design Tool)” in Project Tree Window.
Configure the port. In the Components tab, click "Add component".
Select "Ports" and then click "Finish".
Configure P52 as an output pin and its default output level after reset is 0 (Low level).
To use the "R_BSP_SoftwareDelay" API, please enable this function in r_bsp.
Click “Generate Code” and close Smart Configurator.
Add these user codes to main.c.
Build this project without errors.
Modify the Debug Tool from RL78 Simulator to RL78 E2 Lite.
Double-click “RL78 E2 Lite” to open the Property Window and power the Target Board from the emulator.
Click Debug à Download. You will observe LED2 on this board blinking every second.
Table of Contents |
---|