Verify Hardware Layers
- You can use the modetest application that is included by default in the BSP to verify the hardware layer support of the RZ DRM display drivers.
- In the results returned by modetest, you will see that the overlay image supports the alpha attribute.
- After execution, you can see that the overly image has a translucent effect and is superimposed with the primary layer.
- Simple follow the steps below.
...
{"serverDuration": 124, "requestCorrelationId": "781a1f832f9ca4b9"}