Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

Select "Renesas CC-RX C/C++ Executable Project" or "GCC for Renesas RX C/C++ Excecutable Project"
Click the "Next" button.

Image RemovedImage Added


Type in the project name.  Do not use spaces.
Click the "Next" button.

...

Under the "Debugger" tab, go to the "Connection Settings" subtab. "Power Target From The Emulator (MAX 200ms), select "No".
Click the "Debug" button.
This setting varies depending on the board.
Please refer to the user manual for each board for details.

This procedure allows the user to connect to the debugger and execute the program.

...