If you encounter any issues after the upgrade, please open a support request TICKET.🙌
There are two ways to create a project.
...
View file | |
---|---|
|
|
...
|
The FPB_RX261_LED_Blinky project was created by selecting [Bare Metal - Blinky] on the "Choose a project template" page (see below) when creating a new project.
For information on how to create a project, please refer to the video at the following URL.https://www.renesas.com/en/video/how-create-blinky-project-smart-configurator-e-studiovideo.
Widget Connector width 640 url https://www.youtube.com/watch?v=gfDXL3b9Xmw
...
When creating the FPB_RX261_LED_Blinky project, there are some differences from the video above.
FPB_RX261_LED_Blinky
FPB-RX261
IDE : Renesas Electronics e2 studio 2024-07
...
USB cable (USB Micro-B --- USB Type A) × 1
...
USB cable (USB Micro-B <-> USB Type A) × 1
Windows PC × 1 unit
...
The FPB_RX261_LED_Blinky Project allows customers to change the blinking frequency of the user LED(LED2) cyclically each time the user switch S1 on the FPB-RX261 is pressed.
...