Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.


Some RX MCU peripherals use only fixed interrupt vectors, while some others also use software configurable interrupt vectors.
The software configurable interrupt vectors can configure which interrupt is enabled by the user depending on the application.

How to set the software configurable interrupt depends on the driver you are using.

How to set the software conifugurable interrupt

This is an example for GTCIU2 setting in GPT:

 
To resolve this error, you must configure additional interrupt settings in the "Interrupt tab".
As shown in the figure below, you need to select the interrupt from the corresponding interrupt vector group, INTA or INTB.

Please refer to the "User's Manual: Hardware" of each product to determine whether the interrupt belongs to INTA or INTB.

The table for this information is shown in the following section:

  • Software Configurable Interrupt A Source Select Register n
  • Software Configurable Interrupt B Source Select Register n 

How to verify that the software configurable interrupt is applied

Please check the r_bsp_interrupt_config.h in src/smc_gen/r_config/.


The vector table may be set to blank if the software configurable interrupt setting fails.