If you encounter any issues after the upgrade, please open a support request TICKET.🙌
...
To resolve this error, you must configure additional interrupt settings in the "Interrupt tab".
As shown in the figure below, you need to select the interrupt from the corresponding interrupt vector group, INTA or INTB.
Please also refer to the "User Manual: Hardware" of each product to determine whether the interrupt belongs to INTA or INTB.
(see also the appendix in this page)
This information shows as table in the section as follows in Users Manual:Hardware:
...
If the software configurable interrupt setting is not applied correctly, the vector table may be set as blank.
Please check from this table in the Users manual: Hardware that you will use depens on the software configurable interrupt.