Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

Project name

FPB_RX261_LED_Blinky

Image Modified

Device Settings -> Target Boad

FPB-RX261

Image Modified


1.3 Operating environment for FPB_RX261_LED_Blinky project

...

Select ”Debug Configurtions"

 Image Modified

In the "Debug Configurations" dialog, click "FPB_RX261_LED_Blinkiy HardwareDebug" under "Reness GDB Hardware Debugging".

 Image Modified

Select the "E2 Lite(RX)" in the "Debugger" tab.

 Image Modified

In the "Debugger" tab, in the "Connection Settings" tab, set "Power Target From The Emulator (MAX 200mA)" to "No".

Click the "Debug" button.

 

Image Modified