...
- in case of Code Generator (the component name starts with "Config")
You will get the following error, and it must select the interrupt setting in How to set the software conifugurable interrupt on this page:

- in case of FIT module (the component name starts with "r_")
In general, the software configurable interrupt setting is set automatically.
See also "The software configurable interrupt " setting in the Smart Configurator on this page.
How to set the software conifugurable interrupt
This is an example for GTCIU2 setting in GPT:
...
- Software Configurable Interrupt A Source Select Register n
- Software Configurable Interrupt B Source Select Register n

How to verify that the software configurable interrupt is applied
Please check the r_bsp_interrupt_config.h in src/smc_gen/r_config/.
...