Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

Getting Started

This section describes how to Compile and download the Tes Guilaini Demos on to the RZA3UL.

...

  1. The Project Explorer in the IDE should be empty
  2. Import the TES Projects into the IDE
    1. Right click in the Project Explorer and Select Import
    2. In the Import Dialog select  General -> Existing Projects and Workspaces
    3. In the Import Projects Dialog press the Browes Button then press the Select Folder Button in the popup dialog. Select only the following projects then click Finish.
      1. BSP
      2. SR_GuilianiDemo
  3. Select the SR_GuilianiDemo Project. Right Click and select build. This build will do the following
    1. The Build will attempt a clean first. This will cause an error as there is nothing to clean
    2. Next the Build will first build the BSP Library
    3. Finally the SR_GuilianiDemo will build with no errors
  4. The Generated executable and library files
    1. SR_GuilianiDemo ELF file
      1.   Debug information
    2. SR_GuilianiDemo.sec
      1.   Binary Code
    3. rza3ul_smarc_qspi_ipl.srec
      1. IPL boot loader
    4.   Resources.srec
      1. This is the GUI Widget Resouce file. This is generate the GSE.
  5. Download ( J-Link)
    1. This section refers the Debug Configuration “Renesas GDB Hardware Debug”.
      1.  Connect power to the USBC connector
      2. Connect the J-Link to the Smarc Module. Use the dongle that is provided.
      3. Press and hold the red power button till the power leds are on.
      4. In the menu select Run -> Debug Configurations
      5. In the Debug Configuration Dialog select Renesas GDB Hardware Debug then SR_GuilianiDemo Debug.
        1. NOTE:  If Main Tab has a red dot this indicates the Project with the Debug Configuration was not compiled. Return to step 5.
      6.  A Segger Dialog window will show the progress of the download.

Install the IPL

TBD

Display Configuration

The Display Configuration by default are for a 1080p monitor, however the GUI demo is a Wide VGA demo. When displayed on a PC monitor the resulting image is located in the upper left side of the monitor. This section describes how to configure the RZA3UL Display Unit (DU) for a Wide VGA LCD Display.

Current Tested Displays :

Supported LCDLinkResolution
GeeekPi 5 Inch Capacitive Touch Screen 800x480 HDMI MonitorAmazon800 x 480
DEBO LCD 7 HDMI Entwicklerboardsreichelt.de1024 x 600

RZA3UL Display Settings using FSP.

Step 1) Open the BSP Project FSP Configuration file ( configuration.xml ).

...

DU PropertyGeekPI
Horizontal Total Size1056
Horizontal Active Video Cycles800
Horizontal back porch Cycles216
Horizontal Sync Signal Cycles128
Horizontal Sync Signal PolarityHigh Active
Vertical Total Size628
Vertical Active Video Cycles600
Vertical back porch Cycles27
Vertical Sync Signal Cycles4
Vertical Sync Signal PolarityHigh Active
Data Enable Signal PolarityHigh Active

Display Clock Settings

These steps require modification of the board level display Driver.

...