...
Case1: ROS2 Core (Yocto Native) / Galactic
Case2: ROS2 Core (Docker container) / Humble
...
Simple "Hello World" publisher:
View file
Code Block | ||||||||
---|---|---|---|---|---|---|---|---|
| ||||||||
#!/bin/bash #-# path used to install the SDK: export ROS2_SDK_PATH="/opt/poky/3.1.26_RZV2H_ROS2" export ROS2_SDK_PATH2=${ROS2_SDK_PATH//\//\\/} ### ####### cross-compilation on a Linux PC pip install -U colcon-common-extensions #-# start SDK with unset LD_LIBRARY_PATH source ${ROS2_SDK_PATH}/environment-setup-aarch64-poky-linux export PYTHONPATH="${ROS2_SDK_PATH}/sysroots/x86_64-pokysdk-linux/usr/lib/python3.8/site-packages" export PYTHONPATH="${PYTHONPATH}:${ROS2_SDK_PATH}/sysroots/aarch64-poky-linux/usr/lib64/python3.8/site-packages" export CMAKE_PREFIX_PATH="${ROS2_SDK_PATH}/sysroots/x86_64-pokysdk-linux/usr" export CMAKE_PREFIX_PATH="${CMAKE_PREFIX_PATH}:${ROS2_SDK_PATH}/sysroots/x86_64-pokysdk-linux/usr/lib" export CMAKE_PREFIX_PATH="${CMAKE_PREFIX_PATH}:${ROS2_SDK_PATH}/sysroots/x86_64-pokysdk-linux/usr/lib/cmake" export CMAKE_PREFIX_PATH="${CMAKE_PREFIX_PATH}:${ROS2_SDK_PATH}/sysroots/aarch64-poky-linux/usr" export CMAKE_PREFIX_PATH="${CMAKE_PREFIX_PATH}:${ROS2_SDK_PATH}/sysroots/aarch64-poky-linux/usr/lib64" export CMAKE_PREFIX_PATH="${CMAKE_PREFIX_PATH}:${ROS2_SDK_PATH}/sysroots/aarch64-poky-linux/usr/lib64/cmake" export CMAKE_PREFIX_PATH="${CMAKE_PREFIX_PATH}:${ROS2_SDK_PATH}/sysroots/aarch64-poky-linux/usr/share" export AMENT_PREFIX_PATH="${ROS2_SDK_PATH}/sysroots/aarch64-poky-linux/usr" export AMENT_PREFIX_PATH="${AMENT_PREFIX_PATH}:${ROS2_SDK_PATH}/sysroots/aarch64-poky-linux/usr/lib64" export AMENT_PREFIX_PATH="${AMENT_PREFIX_PATH}:${ROS2_SDK_PATH}/sysroots/aarch64-poky-linux/usr/lib64/cmake" PKGARGS="" if [ $# == 1 ] ; then PKGARGS="--packages-select $1" echo $PKGARGS fi #-# ## cd ros2_ws cp -f cross.cmake.tmp cross.cmake sed -i "s/\/opt\/poky\/3.1.31/$ROS2_SDK_PATH2/g" cross.cmake colcon build --merge-install \ --cmake-force-configure \ --cmake-args \ -DCMAKE_TOOLCHAIN_FILE=${PWD}/cross.cmake \ -DCMAKE_MAKE_PROGRAM=/usr/bin/make \ -DENABLE_PRECOMPILED_HEADERS=OFF \ $PKGARGS |
...