Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

This document describes the procedure for translating YOLOX with DRP-AI Translator v1.80 or later.

Please note the following:

  • Use ONNX in Megvii-BaseDetection/YOLOX (OSS GitHub repository)
  • Cut the post-processing part of the ONNX and use it
  • Run DRP-AI Translator v1.80 or later on Ubuntu 20.04
  • For the Renesas DRP-AI TVM Translator please refer to link 🔗here.

1. Download ONNX

Please run the following command to download the ONNX in Megvii-BaseDetection

$ wget https://github.com/Megvii-BaseDetection/YOLOX/releases/download/0.1.1rc0/yolox_s.onnx

2. Cut post-processing part of ONNX

...

Please edit the following in an editor such as vim, and save it as yolox_s_cut.py.

$ vim yolox_s_cut.py
# yolox_s_cut.py
import onnx
input_path = 'yolox_s.onnx'
output_path = 'yolox_s_wo_post.onnx'
input_names = ['images']
output_names = ['798', '824', '850']
onnx.utils.extract_model(input_path, output_path, input_names, output_names)

As shown in the figure below, please find and specify the output name of Concat before Reshape

Image AddedPlease run yolox_s_cut.py with the following command. If executed successfully, yolox_s_wo_post.onnx will be generated.

$ python3 yolox_s_cut.py

The above output names, 798, 824, and 850, are for YOLOX-s. Please note that different names must be specified for other

YOLOX (e.g. YOLOX-m). As shown in the figure below, please find and specify the output name of Concat before Reshape

of the three outputs of YOLOX.

3. Translate ONNX

Please run DRP-AI Translator using the generated yolox_s_wo_post.onnx. DRP-AI Translator must be v1.80 or later. For

information on how to run DRP-AI Translator, please refer to the User's Manual.

4. Post-processing

The post-processing (Reshape > Concat > Transpose) that is cut this time is the processing that concatinates the data of

three CHW shapes and converts them to HWC shapes.

DRP-AI outputs data in HWC shape by default, so if the three output data are stored in consecutive memory areas, the

same sequence of data as after post-processing is obtained in terms of memory layout.

...

Image Added


Table of Contents