...
...
Image Added Boot Mode Setting |
This demo uses the ZXing Software for decoding. The Renesas DRP (Image Processing Hardware IP) increases the decoding and image processing of the ZXing.
Features:
By default the project is configured for QR Decode. To change the demo to support other barcodes do the following.
Step 1) Open file r_zxing.cpp.
Image Added
Step 2) Modify the Macro definition
Section | |||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Step 3) Do a full recompile of the project
Table of Contents | ||
---|---|---|
|