Besides debugging GR-MANGO with OpenOCD, connecting a Segger j-link is supported as well.
...
Connect the 9-pin J-Link connector:
GR-Mango and J-Link connection
Modify the debug configuration as described for GR-PEACH, but with a different device name for GR-MANGO:
Target Device: R7S921058
e²studio debug configuration for GR-MANGO plus J-Link
Make sure you have installed latest driver from the mbed site here.
Plug the RZ GR board into the PC.
GR-MANGO |
GR-PEACH |
MBED USB Debug Port | GR-LYCHEE |
MBED USB Debug connector |
Open the Windows OS Device Manager. You should see the device here.