Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

DRM Block Diagram.pngImage RemovedImage Added

Verify Hardware Layers

  • You can use the modetest application that is included by default in the BSP to verify the hardware layer support of the RZ DRM display drivers.
  • In the results returned by modetest, you will see that the overlay image supports the alpha attribute.
  • After execution, you can see that the overly image has a translucent effect and is superimposed with the primary layer.
  • Simple follow the steps below.

...

For example, according to the return result of modetest on a RZ/G2L EVK, RZ/G2L has 2 physical planes.

Expand

...

titleExample modetest output on a RZ/G2L EVK

...

root@smarc-rzg2l:~# modetest -M rcar-du
Encoders:
id      crtc    type    possible crtcs  possible clones
38      37      none    0x00000001      0x00000001
44      0       Virtual 0x00000001      0x00000002

Connectors:
id      encoder status          name            size (mm)       modes   encoders
39      38      connected       HDMI-A-1        0x0             26      38
  modes:
        index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
  #0 1280x800 59.91 1280 1328 1360 1440 800 803 807 823 71000 flags: phsync, pvsync; type: preferred, driver
  #1 1920x1080 60.00 1920 2008 2052 2200 1080 1084 1089 1125 148500 flags: phsync, pvsync; type: driver
  #2 1920x1080 60.00 1920 2008 2052 2200 1080 1084 1089 1125 148500 flags: phsync, pvsync; type: driver
  #3 1920x1080 59.94 1920 2008 2052 2200 1080 1084 1089 1125 148352 flags: phsync, pvsync; type: driver
  #4 1280x1024 60.02 1280 1328 1440 1688 1024 1025 1028 1066 108000 flags: phsync, pvsync; type: driver
  #5 1280x960 60.00 1280 1376 1488 1800 960 961 964 1000 108000 flags: phsync, pvsync; type: driver
  #6 1280x800 60.00 1280 1316 1324 1324 800 816 824 832 66090 flags: phsync, pvsync; type: driver
  #7 1152x864 75.00 1152 1216 1344 1600 864 865 868 900 108000 flags: phsync, pvsync; type: driver
  #8 1280x720 60.00 1280 1390 1430 1650 720 725 730 750 74250 flags: phsync, pvsync; type: driver
  #9 1280x720 59.94 1280 1390 1430 1650 720 725 730 750 74176 flags: phsync, pvsync; type: driver
  #10 1024x768 75.03 1024 1040 1136 1312 768 769 772 800 78750 flags: phsync, pvsync; type: driver
  #11 1024x768 70.07 1024 1048 1184 1328 768 771 777 806 75000 flags: nhsync, nvsync; type: driver
  #12 1024x768 60.00 1024 1048 1184 1344 768 771 777 806 65000 flags: nhsync, nvsync; type: driver
  #13 800x600 75.00 800 816 896 1056 600 601 604 625 49500 flags: phsync, pvsync; type: driver
  #14 800x600 72.19 800 856 976 1040 600 637 643 666 50000 flags: phsync, pvsync; type: driver
  #15 800x600 60.32 800 840 968 1056 600 601 605 628 40000 flags: phsync, pvsync; type: driver
  #16 800x600 56.25 800 824 896 1024 600 601 603 625 36000 flags: phsync, pvsync; type: driver
  #17 720x480 60.00 720 736 798 858 480 489 495 525 27027 flags: nhsync, nvsync; type: driver
  #18 720x480 60.00 720 736 798 858 480 489 495 525 27027 flags: nhsync, nvsync; type: driver
  #19 720x480 59.94 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
  #20 720x480 59.94 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
  #21 720x480 59.94 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
  #22 640x480 75.00 640 656 720 840 480 481 484 500 31500 flags: nhsync, nvsync; type: driver
  #23 640x480 72.81 640 664 704 832 480 489 492 520 31500 flags: nhsync, nvsync; type: driver
  #24 640x480 60.00 640 656 752 800 480 490 492 525 25200 flags: nhsync, nvsync; type: driver
  #25 640x480 59.94 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type: driver
  props:
        1 EDID:
                flags: immutable blob
                blobs:

                value:
                        00ffffffffffff0020641d7b01000000
                        201b0103800000780ae0ce9e59579723
                        124c542fce00010181808140714f0101
                        010101010101bc1b00a0502017303020
                        340000000000001e000000ff004c544d
                        31320a20202020202020000000fd0032
                        551f4f0b000a202020202020000000fc
                        00504a343032442d320a20202020018d
                        02031af1479005040302071623090707
                        65030c00100083010000023a80187138
                        2d40582c450007442100001e011d8018
                        711c1620582c250007442100009ed119
                        002c5020203024080804510e1100001e
                        8c0ad08a20e02d10103e960007442100
                        00180000000000000000000000000000
                        00000000000000000000000000000012
        2 DPMS:
                flags: enum
                enums: On=0 Standby=1 Suspend=2 Off=3
                value: 0
        5 link-status:
                flags: enum
                enums: Good=0 Bad=1
                value: 0
        6 non-desktop:
                flags: immutable range
                values: 0 1
                value: 0
        4 TILE:
                flags: immutable blob
                blobs:

                value:
        20 CRTC_ID:
                flags: object
                value: 37

CRTCs:
id      fb      pos     size
37      47      (0,0)   (1280x800)
  #0 1280x800 59.91 1280 1328 1360 1440 800 803 807 823 71000 flags: phsync, pvsync; type: preferred, driver
  props:
        22 ACTIVE:
                flags: range
                values: 0 1
                value: 1
        23 MODE_ID:
                flags: blob
                blobs:

                value:
                        58150100000530055005a00500002003
                        23032703370300003c00000005000000
                        48000000313238307838303000000000
                        00000000000000000000000000000000
                        00000000
        19 OUT_FENCE_PTR:
                flags: range
                values: 0 18446744073709551615
                value: 0
        24 VRR_ENABLED:
                flags: range
                values: 0 1
                value: 0

Planes:
id      crtc    fb      CRTC x,y        x,y     gamma size      possible crtcs
32      37      47      0,0             0,0     0               0x00000001
  formats: RGB8 AR12 XR12 AR15 XR15 RG16 BG24 RG24 BA24 BX24 AR24 XR24 UYVY YUYV YVYU NV12 NV21 NV16 NV61 YU12 YV12 YU16 YV16 YU24 YV24
  props:
        8 type:
                flags: immutable enum
                enums: Overlay=0 Primary=1 Cursor=2
                value: 1
        17 FB_ID:
                flags: object
                value: 47
        18 IN_FENCE_FD:
                flags: signed range
                values: -1 2147483647
                value: -1
        20 CRTC_ID:
                flags: object
                value: 37
        13 CRTC_X:
                flags: signed range
                values: -2147483648 2147483647
                value: 0
        14 CRTC_Y:
                flags: signed range
                values: -2147483648 2147483647
                value: 0
        15 CRTC_W:
                flags: range
                values: 0 2147483647
                value: 1280
        16 CRTC_H:
                flags: range
                values: 0 2147483647
                value: 800
        9 SRC_X:
                flags: range
                values: 0 4294967295
                value: 0
        10 SRC_Y:
                flags: range
                values: 0 4294967295
                value: 0
        11 SRC_W:
                flags: range
                values: 0 4294967295
                value: 83886080
        12 SRC_H:
                flags: range
                values: 0 4294967295
                value: 52428800
        33 zpos:
                flags: immutable range
                values: 0 0
                value: 0
34      0       0       0,0             0,0     0               0x00000001
  formats: RGB8 AR12 XR12 AR15 XR15 RG16 BG24 RG24 BA24 BX24 AR24 XR24 UYVY YUYV YVYU NV12 NV21 NV16 NV61 YU12 YV12 YU16 YV16 YU24 YV24
  props:
        8 type:
                flags: immutable enum
                enums: Overlay=0 Primary=1 Cursor=2
                value: 0
        17 FB_ID:
                flags: object
                value: 0
        18 IN_FENCE_FD:
                flags: signed range
                values: -1 2147483647
                value: -1
        20 CRTC_ID:
                flags: object
                value: 0
        13 CRTC_X:
                flags: signed range
                values: -2147483648 2147483647
                value: 0
        14 CRTC_Y:
                flags: signed range
                values: -2147483648 2147483647
                value: 0
        15 CRTC_W:
                flags: range
                values: 0 2147483647
                value: 0
        16 CRTC_H:
                flags: range
                values: 0 2147483647
                value: 0
        9 SRC_X:
                flags: range
                values: 0 4294967295
                value: 0
        10 SRC_Y:
                flags: range
                values: 0 4294967295
                value: 0
        11 SRC_W:
                flags: range
                values: 0 4294967295
                value: 0
        12 SRC_H:
                flags: range
                values: 0 4294967295
                value: 0
        35 alpha:
                flags: range
                values: 0 65535
                value: 65535
        36 zpos:
                flags: range
                values: 1 1
                value: 1

Frame buffers:
id      size    pitch

Below is an example of an RZ/G2L connected to a 1280x800 MHDI LCD. There are 2 IDSs for "Planes" ('32' and '34') because there are 2 hardware layers in the RZ/G2L LCD display controller.

...