Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.
HTML<font size=6><B>RA Series

RA Series 32-bit

MCUs</B></font>

MCUsImage Added

Introduction

Image RemovedThis page is for the Renesas RA family of MCUs. The main goal is to make the information about RA MCUs friendly, easy to access for embedded developers.

The links below can be used to get familiar with Renesas RA MCUs. 

Getting Started with RA

Here are the resources for RA MCUs on Renesas GitHub site.

  • Flexible Software Package (FPSFSP)
  • Example Projects (EPs)
  • Application Project (APs

Other resources on Renesas Website.  Links below are pre-configured searches.  You can modify them as needed.  

e2studio is the Renesas supported IDE. You can also use EWARM and Keil IDEs.  Supported   Supported toolchains are Arm GNU Toolchain, LLVM Embedded Toolchain for Arm, IAR Compiler, and Arm Compiler.  3rd party IDEs and toolchains are supported by respective partner companies.  

Each FSP version and supported tools are available from the Releases page.  Bundled platform installers are available at the bottom of each FSP version under Assets section.   

Boards

Official Renesas RA series boards are available available here.  Each board has its landing page and most have the following information. 

  • Board Quick Start Guide
  • Board User's Manual
  • Board Design Package 

IBIS models can be found here

Your First RA Project

Please holder for Blinky project. 

Tips and Tricks

Section
bordertrue
Column

Debugger connectivity with ID code protection

Placeholder for setting ID codes

Section
bordertrue
Column

Multiple pin configuration

Placeholder for creating multiple pin configurations

Run-time SPI configuration

Placeholder for configuring SPI channel for different targets

Debugger connectivity with TrustZone devices

Placeholder for serial programming interface requirements to configure TrustZone IDAU registers 

Bugs and Workarounds

Section
bordertrue

gldjgldjgldjgldj

Section
bordertrue

fkshfksfkshfkshf

section

This is your first RA project, designed to blink the LEDs on the EK-RA8D1 board.  It serves as an introduction to e2studio, the RA project creator, and the FSP Configurator.  The process outlined applies to all official Renesas RA series boards.  Additionally, this project provides a simple way to verify that your development environment is set up correctly and that all necessary tools are functioning properly.

Your First RA Project

Tips and Tricks

RA Tips and Tricks page page contains many useful information and how to notes on everything RA.  We update the page regularly so come and check it often.   

Known Issues and Workarounds

RA Issues page lists known bugs and possible workarounds for HW, SW, and tools.  

RA Specific Topics

This is to discuss specific topics for RA.  Each topic discussed here can be detailed and lengthy.  Therefore, RA Specific Topics page serves as a table of contents with a short description of the topics followed by a dedicated page for that subject.   




Table of Contents