Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

  • The Link Status input pin (LINKSTA) is not used. The driver instead relies on the PHY to inform it that the link is up by using in-band status messages on the RGMII lines.
  • Do not forget to set the correct voltage levels for the pins (3.3v, 1.5v, etc..) in the device tree in the pinctrl node.
    • You use the syntax "power-source = <3300>;" when you declare the pins for Ethernet. If an Ethernet PHY supports multiple voltages (3.3v or 1.8v), then choose the lower voltage because the Electrical Characteristics are better.
    • Refer to the pinctrl documentation in the kernel for more info.
    • Documentation/devicetree/bindings/pinctrl/renesas,rzg2l-pinctrl.yaml
    • Documentation/devicetree/bindings/pinctrl/renesas,pcf.yaml
  • In the Device Tree, the MDIO address is set by @x and the "reg =<x>;" For example, MDIO address of 0:
	phy0: ethernet-phy@0 {
		reg = <0>;
  • If using MII (not RGMII), do not include output-enable; in txc{  } in your Device Tree. For RGMII, TX_CLK is always an output. But for MII, TX_CLK pin needs to be an input, so output-enable should not be set.



Device Tree Examples

Expand
titleExample of enabling MII mode for RZ/G2L

Ethernet node for MII mode

&eth0 {
	pinctrl-0 = <&eth0_mii_pins>;
	pinctrl-names = "default";
	phy-handle = <&phy0>;
	phy-mode = "mii";
	status = "okay";

	phy0: ethernet-phy@7 {
		compatible = "ethernet-phy-id0022.1640",
			     "ethernet-phy-ieee802.3-c22";
		reg = <7>;
		rxc-skew-psec = <2400>;
		txc-skew-psec = <2400>;
		rxdv-skew-psec = <0>;
		txdv-skew-psec = <0>;
		rxd0-skew-psec = <0>;
		rxd1-skew-psec = <0>;
		rxd2-skew-psec = <0>;
		rxd3-skew-psec = <0>;
		txd0-skew-psec = <0>;
		txd1-skew-psec = <0>;
		txd2-skew-psec = <0>;
		txd3-skew-psec = <0>;

		interrupt-parent = <&pinctrl>;
		interrupts = <RZG2L_GPIO(1, 0) IRQ_TYPE_LEVEL_LOW>;
	};
};

&eth1 {
	pinctrl-0 = <&eth1_mii_pins>;
	pinctrl-names = "default";
	phy-handle = <&phy1>;
	phy-mode = "mii";
	status = "okay";

	phy1: ethernet-phy@7 {
		compatible = "ethernet-phy-id0022.1640",
			     "ethernet-phy-ieee802.3-c22";
		reg = <7>;
		rxc-skew-psec = <2400>;
		txc-skew-psec = <2400>;
		rxdv-skew-psec = <0>;
		txdv-skew-psec = <0>;
		rxd0-skew-psec = <0>;
		rxd1-skew-psec = <0>;
		rxd2-skew-psec = <0>;
		rxd3-skew-psec = <0>;
		txd0-skew-psec = <0>;
		txd1-skew-psec = <0>;
		txd2-skew-psec = <0>;
		txd3-skew-psec = <0>;

		interrupt-parent = <&pinctrl>;
		interrupts = <RZG2L_GPIO(1, 1) IRQ_TYPE_LEVEL_LOW>;
	};
};


Pin Setup

&pinctrl {

	eth0_mii_pins: eth0 {
		pinmux = <RZG2L_PORT_PINMUX(28, 1, 1)>, /* ET0_LINKSTA */
			 <RZG2L_PORT_PINMUX(27, 1, 1)>, /* ET0_MDC */
			 <RZG2L_PORT_PINMUX(28, 0, 1)>, /* ET0_MDIO */
			 <RZG2L_PORT_PINMUX(20, 0, 1)>, /* ET0_TXC */
			 <RZG2L_PORT_PINMUX(20, 1, 1)>, /* ET0_TX_CTL */
			 <RZG2L_PORT_PINMUX(20, 2, 1)>, /* ET0_TXD0 */
			 <RZG2L_PORT_PINMUX(21, 0, 1)>, /* ET0_TXD1 */
			 <RZG2L_PORT_PINMUX(21, 1, 1)>, /* ET0_TXD2 */
			 <RZG2L_PORT_PINMUX(22, 0, 1)>, /* ET0_TXD3 */
			 <RZG2L_PORT_PINMUX(22, 1, 1)>,	/* ETH0_TX_ERR */
			 <RZG2L_PORT_PINMUX(23, 0, 1)>,	/* ETH0_TX_COL */
			 <RZG2L_PORT_PINMUX(23, 1, 1)>, /* ETH0_TX_CRS */
			 <RZG2L_PORT_PINMUX(24, 0, 1)>, /* ET0_RXC */
			 <RZG2L_PORT_PINMUX(24, 1, 1)>, /* ET0_RX_CTL */
			 <RZG2L_PORT_PINMUX(25, 0, 1)>, /* ET0_RXD0 */
			 <RZG2L_PORT_PINMUX(25, 1, 1)>, /* ET0_RXD1 */
			 <RZG2L_PORT_PINMUX(26, 0, 1)>, /* ET0_RXD2 */
			 <RZG2L_PORT_PINMUX(26, 1, 1)>, /* ET0_RXD3 */
			 <RZG2L_PORT_PINMUX(27, 0, 1)>; /* ETH0_RX_ERR */
	};

	eth1_mii_pins: eth1 {
		pinmux = <RZG2L_PORT_PINMUX(37, 2, 1)>, /* ET1_LINKSTA */
			 <RZG2L_PORT_PINMUX(37, 0, 1)>, /* ET1_MDC */
			 <RZG2L_PORT_PINMUX(37, 1, 1)>, /* ET1_MDIO */
			 <RZG2L_PORT_PINMUX(29, 0, 1)>, /* ET1_TXC */
			 <RZG2L_PORT_PINMUX(29, 1, 1)>, /* ET1_TX_CTL */
			 <RZG2L_PORT_PINMUX(30, 0, 1)>, /* ET1_TXD0 */
			 <RZG2L_PORT_PINMUX(30, 1, 1)>, /* ET1_TXD1 */
			 <RZG2L_PORT_PINMUX(31, 0, 1)>, /* ET1_TXD2 */
			 <RZG2L_PORT_PINMUX(31, 1, 1)>, /* ET1_TXD3 */
			 <RZG2L_PORT_PINMUX(32, 0, 1)>, /* ETH1_TX_ERR */
			 <RZG2L_PORT_PINMUX(32, 1, 1)>, /* ETH1_TX_COL */
			 <RZG2L_PORT_PINMUX(33, 0, 1)>, /* ETH1_TX_CRS */
			 <RZG2L_PORT_PINMUX(33, 1, 1)>, /* ET1_RXC */
			 <RZG2L_PORT_PINMUX(34, 0, 1)>, /* ET1_RX_CTL */
			 <RZG2L_PORT_PINMUX(34, 1, 1)>, /* ET1_RXD0 */
			 <RZG2L_PORT_PINMUX(35, 0, 1)>, /* ET1_RXD1 */
			 <RZG2L_PORT_PINMUX(35, 1, 1)>, /* ET1_RXD2 */
			 <RZG2L_PORT_PINMUX(36, 0, 1)>, /* ET1_RXD3 */
			 <RZG2L_PORT_PINMUX(36, 1, 1)>; /* ETH1_RX_ERR */
	};
};  
, 0, 1)>, /* ET1_RXD3 */
			 <RZG2L_PORT_PINMUX(36, 1, 1)>; /* ETH1_RX_ERR */
	};
};  

PCIe

Linux Drivers

  • RZ/G2, RZ/G3

Host:

    • drivers/pci/controller/pcie-rcar.c
    • drivers/pci/controller/pcie-rcar.h
    • drivers/pci/controller/pcie-rcar-host.c
    • Documentation/devicetree/bindings/pci/rcar-pci.txt
    • CONFIG_PCIE_RCAR_HOST=y

End Point:

    • drivers/pci/controller/pcie-rcar.c
    • drivers/pci/controller/pcie-rcar.h
    • drivers/pci/controller/pcie-rcar-ep.c
    • Documentation/devicetree/bindings/pci/rcar-pci-ep.yaml
    • CONFIG_PCIE_RCAR_EP=y


Notes

  • PCIe testing using SSD:
  1. Enable Kernel configuration:

         PCIe was enabled by default in the RZ/G2 BSP. But you need to modify the kernel menuconfig to add support for NVME M.2 SDD.

         Example to modify kernel in yocto is:

$ bitbake -c menuconfig virtual/kernel

Once menuconfig appears, enable device driver for nvme support and save the changes.

Then build the kernel with new configuration.

$ bitbake linux-renesas -fc compile
$ bitbake linux-renesas -fc install
$ bitbake linux-renesas -fc deploy

       Once the built is done, update your kernel and device tree with newly built.

    2. Connect the SSD adapter board to RZ/G2H PCIe slot and check PCIe:

$ root@hihope-rzg2h:~# lspci
00:00.0 PCI bridge: Renesas Technology Corp. Device 0025
01:00.0 Non-Volatile memory controller: Samsung Electronics Co Ltd NVMe SSD Controller SM981/PM981/PM983
$ root@hihope-rzg2h:~# lsblk
NAME         MAJ:MIN RM   SIZE RO TYPE MOUNTPOINT
mmcblk0      179:0    0  29.7G  0 disk
`-mmcblk0p1  179:1    0  29.7G  0 part
mmcblk0boot0 179:8    0  31.5M  1 disk
mmcblk0boot1 179:16   0  31.5M  1 disk
mmcblk1      179:24   0  14.9G  0 disk
|-mmcblk1p1  179:25   0   512M  0 part
`-mmcblk1p2  179:26   0   1.8G  0 part /
nvme0n1      259:0    0 238.5G  0 disk   # recognized the NVME SSD

    3. Create a partition on the nvme to use

$ root@hihope-rzg2h:~# fdisk /dev/nvme0n1
Choose "n" to create a new partition
Choose "P" then "1" to create a new primary partition
Use defaults for the sector numbers
Then "w" to write the data to the disk

    After partition, "lsblk" command shows this:

$ root@hihope-rzg2h:~# lsblk
NAME         MAJ:MIN RM   SIZE RO TYPE MOUNTPOINT
mmcblk0      179:0    0  29.7G  0 disk
`-mmcblk0p1  179:1    0  29.7G  0 part
mmcblk0boot0 179:8    0  31.5M  1 disk
mmcblk0boot1 179:16   0  31.5M  1 disk
mmcblk1      179:24   0  14.9G  0 disk
|-mmcblk1p1  179:25   0   512M  0 part
`-mmcblk1p2  179:26   0   1.8G  0 part /
nvme0n1      259:0    0 238.5G  0 disk
`-nvme0n1p1  259:1    0 238.5G  0 part   # new partition

    4. Create the filesystem:

$ root@hihope-rzg2h:~# mkfs -t ext4 /dev/nvme0n1p1

   5. Create mount point:

$ root@hihope-rzg2h:~# mkdir /mnt/nvme
root@hihope-rzg2h:~# mount /dev/nvme0n1p1 /mnt/nvme
[  970.462102] EXT4-fs (nvme0n1p1): recovery complete
[  970.468717] EXT4-fs (nvme0n1p1): mounted filesystem with ordered data mode. Opts: (null)

   6. Create file to write/read:

$ root@hihope-rzg2h:~# touch /mnt/nvme/testfile

   7. Example for PCIe performance measured on PCIe Slot port of RZ/G2H, and with a Samsung NVMe SSD PM981a:

root@hihope-rzg2h:~# echo 3 > /proc/sys/vm/drop_caches  # to drop both page cache and dentries/inodes
[  498.378440] sh (620): drop_caches: 3
root@hihope-rzg2h:~# dd if=/dev/zero of=/mnt/nvme/testfile bs=200M count=50 oflag=direct
50+0 records in
50+0 records out
10485760000 bytes (10 GB, 9.8 GiB) copied, 29.009 s, 361 MB/s
root@hihope-rzg2h:~# echo 3 > /proc/sys/vm/drop_caches
[  616.062183] sh (620): drop_caches: 3
root@hihope-rzg2h:~# dd if=/mnt/nvme/testfile of=/dev/null bs=200M  count=50 iflag=direct
50+0 records in
50+0 records out
10485760000 bytes (10 GB, 9.8 GiB) copied, 24.6171 s, 426 MB/s

USB

Linux Drivers

  • RZ/G2H, G2M, G2N, G2E:
  • RZ/G2L, G2LC, G2UL, V2L:

...

  • RZ/G2H, G2M, G2N, G2E:
    • CONFIG_xxxPWM_RZ_MTU3=y
    • drivers/pwm/pwm-rz-mtu3.c
  • RZ/G2L, G2LC, G2UL, V2L:
    • CONFIG_xxxGPT_RZG2L=y
    • drivers/pwm/gpt-rzg2l.c

Notes

Device Tree Examples

...

  • RZ/G2H, G2M, G2N, G2E:
    • drivers/thermal/rcar_gen3__thermal.c
    • CONFIG_RCAR_GEN3_THERMAL=y
  • RZ/G2L, G2LC, G2UL, V2L:
    • drivers/thermal/rzg2l_thermal.c
    • CONFIG_RZG2L_THERMAL=y
  • RZ/V2H
    • Supported on AI_SDK 5.0 and later
    • Enabled by default
    • CONFIG_RZG2L_THERMAL=y

Notes

...