Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.


Section
Column
HTML
<style> .confluenceTd {border: none !important;} </style>

Individual Topics

Topics

...

BSP Download links and extra information

...


📇 Yocto

Common issues, suggestions, examples

...


🎛️ Hardware

DDR, Clocks, Timers, etc..

...


📷 Camera

Setup info, capture examples

...


🎨 Graphics

GUI, GPU, video encode/decode, HTML


🖼️ Wayland/Weston

Helpful hints about using Weston

...


🐧 Kernel

Kernel config, Dynamic Power, GPIO, drivers


🔑

...

...


🥾 u-boot

Helpful info, GPIO control


🌳

...

Device Tree and Device Drivers

How to enable drivers, Device Tree examples

...


🚧 RZ

...

Linux BSP Porting

Hints on porting to a new board


...

RZ/G2 Flash Programming

Ideas for programming Flash Memory

...


🐛 Debugging

JTAG, OpenOCD, Eclipse

...


🧠 AI and ML

Open Source AI frameworks


Image Modified⏭️ GStreamer

Hints and

...

Examples


🎥

...

Demo Videos

A collection of video links

...


📡 Communications

RS-485, SPI, Ethernet, LBSC, etc...






General Learning

This section is for general information regarding Linux, Software Development and Open Source.

🐧 Working with Linux

• General Embedded Linux Information


♻️ Open Source

• Explanation and Information on Open Source packages that are relevant to Renesas (Yocto, GStreamer, Weston, etc...)







Column

Image Added

Image Added