If you encounter any issues after the upgrade, please open a support request TICKET.🙌
Image RemovedThis page is for the Renesas RX family of MCUs. The main goal is to make the information about RX MCUs friendly, easy to access for embedded developers.fhkjfskhf
The links below can be used to get familiar with Renesas RX MCUs.
Here are the resources for RX MCUs on Renesas GitHub site.Website.
Other resources on Renesas Website. Links below are pre-configured searches. You can modify them as needed.
e2studio is the Renesas supported IDE. You can also use EWARM and Keil IDEs. Supported toolchains are Arm GNU Toolchain, LLVM Embedded Toolchain for Arm, IAR Compiler, and Arm Compiler.
Each FSP version and supported tools are available from the Releases page. Bundled platform installers are available at the bottom of each FSP version under Assets section.
Official Renesas RX series boards are available here. There are several types of boards are available:
RX series boards are available here. Each board has its landing page and most have the following information.
Please holder for Blinky project.
The following webpage describes the procedure for creating a C project using the Smart Configurator in e2studio IDE.
RX Tips and Tricks page contains many useful information and how to notes on everything RX. We update the page regularly so come and check it often.
This section is to discuss specific topics for RX. Each topic discussed here can be detailed and lengthy. Therefore, RX Specific Topics page serves as a table of contents with a short description of the topics followed by a dedicated page for that subject. ==================== END OF COMMON MCU PAGE ======================
Table of Contents |
---|