Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

Verify Hardware Layers

  • You can use the modetest application that is included by default in the BSP to verify the hardware layer support of the RZ DRM display drivers.
  • In the results returned by modetest, you will see that the overlay image supports the alpha attribute.
  • After execution, you can see that the overly image has a translucent effect and is superimposed with the primary layer.
  • Simple follow the steps below.

...