Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

Background

Some RX MCU peripherals use only fixed interrupt vectors, while some others also use software configurable interrupt vectors.
The software configurable interrupt vectors can configure select which interrupt is enabled by the user depending on the application.
And, the two kinds of . The software configurable interrupt setting is available, it separates as the using source clock these are PCLKA and PCLCBis separated into two types for each clock source (PCKLA and PCLKB) as INTA and INTB.

Image ModifiedImage Modified


How to set the software configurable interrupt depends on the driver you are using.

How to set the software

...

configurable interrupt

This is an example of how to remove the error for the GTCIU2 setting in GPT:

 
To resolve this error, you must configure additional interrupt settings in the "Interrupt Interrupts tab".
As shown in the figure below, you need to select the interrupt from the corresponding interrupt vector group, INTA or INTB.

Image RemovedImage Added

Please refer to the "User's Manual: Hardware" of each product to determine whether the interrupt belongs to INTA or INTB.

...

  • Software Configurable Interrupt A Source Select Register n
  • Software Configurable Interrupt B Source Select Register n 

Image RemovedImage Added

How to verify that the software configurable interrupt is applied

Please check the r_bsp_interrupt_config.h in src/smc_gen/r_config/.


The If software configurable interrupt settings fails, the vector table may be set to blank. if you faced this case, please handle the interrupt setting by using How to set the software configurable interrupt setting fails.