If you encounter any issues after the upgrade, please open a support request TICKET.🙌
Background
Some RX MCU peripherals use only fixed interrupt vectors, while some others also use software configurable interrupt vectors.
The software configurable interrupt vectors can configure select which interrupt is enabled by the user depending on the application.
The software configurable interrupt is separated into two types for each clock source (PCKLA and PCLKB) as INTA and INTB.
...
...
This is an example of how to remove the error for the GTCIU2 setting in GPT:
To resolve this error, you must configure additional interrupt settings in the "Interrupt Interrupts tab".
As shown in the figure below, you need to select the interrupt from the corresponding interrupt vector group, INTA or INTB.
Please refer to the "User's Manual: Hardware" of each product to determine whether the interrupt belongs to INTA or INTB.
...
Please check the r_bsp_interrupt_config.h in src/smc_gen/r_config/.
The If software configurable interrupt settings fails, the vector table may be set to blank. if you faced this case, please handle the interrupt setting by using How to set the software configurable interrupt setting fails.