If you encounter any issues after the upgrade, please open a support request TICKET.🙌
This page shows you how to create an RX project. As an example, we use an FPB-RX261 board but you can use any official Renesas RX board.
The Blinky project is also a good way to verify your tools installation before you start diving into more advanced projects.
Go to "File2 File" >> "New" >> "Renesas C/C++ Project >> Renesas RX"
Select "Renesas CC-RX C/C++ Executable Project" or "GCC for Renesas RX C/C++ Excecutable Project"
Click the "Next" button.
Type in the project name. Do not use spaces.
Click the "Next" button.
In the ”Select toolchain, device & debug settings" windowUnder ”Toolchain", "Target Board", and "Configurations", select your toolchain, target board, and debug configuration.
"Target Device" is auto populated from "Target Board" selection.
Click the "Next" button.
In the "Select Coding Assistant Settings" window, select "Use Smart Configurator".
Click the "Next" button.
In the "Choose a project template" window, select "Bare Metal - Blinky".
This template includes simple source code sample application code to blink LED on an official Renesas RX board.
Click the "Finish" button.
If you see the window below, check the "Remember my decision" box and click the "Open Perspective" button.
This opens the Smart Configurator perspective that allows you to configure your project visually.
You should see a flashing project The project you created appears in the Project Explorer pane. At the bottom of the Smart Configurator view are the tabs: "Overview", "Board", "Clocks", "System", "Components", "Pins" and "Interrupts". These tabs are useful for configuring the project and adding new FIT modules.
For more information, click the "User's Guide" button.
The newly created project contains all the necessary drivers and configuration.
It also includes sample application code to blink LED.
The project can be built and debugged.
Go to "Project" >> "Build Project".
You should see your project is built without errors.
This section explains an example of connecting a debugger using the FPB-RX261 board.
To debug and program with the FPB-RX261, you must set it to Debug on-board mode.
To enter Debug on-board mode, short pins 2 and 3 of the pin header jumper J4.
Then connect the FPB-RX261 to the PC with the USB cable and change the e2studio settings as follows.
Select ”Debug Configurtions"
...
Under the "Debugger" tab, go to the "Connection Settings" subtab. "Power Target From The Emulator (MAX 200ms), select "No".
Click the "Debug" button.
This setting varies depending on the board.
Please refer to the user manual for each board for details.
This procedure allows the user to connect to the debugger and execute the program.
...
If you see the window below, check the "Remember my decision" box and click "Switch" button.
This switches the view to the Debug perspective and rearranges your panes for easy debugging.
You should see window below The following window will appear. In editor pane, source code shows the reset startup code.
Go to "Run" >> "Resume". Execution stops at main(). Go to "Run" >> "Resume" again.
The LED on your board should now be blinking.
...