HTML |
---|
<! To make a ToC move/scroll with the page >
<style> .toc-macro {position: static !important;} </style>
<! Make the ToC in-line (not float on the right) >
<style> .toc-macro {float: none !important;} </style>
<! To make a ToC wider >
<style> .toc-macro {width: 350px !important;} </style>
<! Transparent background (no color) >
<style> .toc-macro {background: transparent !important;} </style>
<! To make a ToC Font Size bigger. Default font-size: 15px. Default line-height: 1.6 >
<style> .toc-item-body {font-size: 18px !important;} </style> |
Table of Contents |
---|
This page is an an example for RZ/G2L. It is based on using VLP 3.0.6.
Qt 5.15.2 can run on various backends. The EGLFS and Wayland backends are widely used. Here, we will talk about how to build and integrate Qt 5.15.2 with EGLFS and Wayland backends support based on VLP 3.0.6.
The default Yocto SDK of VLP 3.0.6 can only support the Qt with Wayland backend building. So the patch for the Qt 5.6.3(Qt version of VLP 3.0.6) recipe must be applied.
...
Note: The Qt 5.6.3 with EGLFS backend support is ready. If you only need Qt 5.6.3, you can skip the following steps.
2.1) Get the Qt source code
# cd to any directory under ubuntu
cd <work-dir>
# download Qt 5.15.2 source code
wget https://download.qt.io/archive/qt/5.15/5.15.2/single/qt-everywhere-src-5.15.2.tar.xz
# decompress
tar -xvf qt-everywhere-src-5.15.2.tar.xz
...
#
# qmake configuration for building with aarch64-linux-gnu-g++
#
MAKEFILE_GENERATOR = UNIX
CONFIG += incremental
QMAKE_INCREMENTAL_STYLE = sublib
QMAKE_LIBS_EGL += -lEGL
QMAKE_LIBS_OPENGL_ES2 += -lGLESv2 -lEGL
QMAKE_CFLAGS = -march=armv8-a -mtune=cortex-a55
QMAKE_CXXFLAGS = $$QMAKE_CFLAGS
EGLFS_DEVICE_INTEGRATION = eglfs_kms
include(../common/linux.conf)
include(../common/gcc-base-unix.conf)
include(../common/g++-unix.conf)
# modifications to g++.conf
QMAKE_CC = aarch64-poky-linux-gcc
QMAKE_CXX = aarch64-poky-linux-g++
QMAKE_LINK = aarch64-poky-linux-g++
QMAKE_LINK_SHLIB = aarch64-poky-linux-g++
# # modifications to linux.conf
QMAKE_AR = aarch64-poky-linux-ar cqs
QMAKE_OBJCOPY = aarch64-poky-linux/aarch64-poky-linux-objcopy
QMAKE_NM = aarch64-poky-linux/aarch64-poky-linux-nm -P
QMAKE_STRIP = aarch64-poky-linux-strip
load(qt_config)
...
#!/bin/bash
if [ "x" == "x$1" ]; then
echo "No qt source dir specified"
exit 0
fi
PWD=`pwd`
OUTPUT=$PWD/output
YOCTOSDK=/opt/poky/3.1.31/sysroots
ROOTFS=$YOCTOSDK/aarch64-poky-linux
export PATH=$YOCTOSDK/x86_64-pokysdk-linux/usr/bin/aarch64-poky-linux:$PATH
export PKG_CONFIG_LIBDIR=$YOCTOSDK/aarch64-poky-linux/usr/lib64/pkgconfig
rm -rf $OUTPUT/*
cd $1
./configure -v -extprefix $OUTPUT -opensource -release -optimized-qmake -confirm-license -xplatform linux-aarch64-gnu-g++ -sysroot $ROOTFS -shared -silent -no-pch -no-rpath -pkg-config -no-pulseaudio -no-alsa -no-evdev -no-sse2 -no-sse3 -no-cups -dbus -make examples -compile-examples -no-fontconfig -opengl es2 -egl -eglfs -no-glib -no-harfbuzz -no-iconv -icu -system-libjpeg -kms -gbm -system-libpng -no-libproxy -make libs -linuxfb -no-mtdev -no-openssl -no-openvg -qt-pcre -sm -no-sql-db2 -no-sql-ibase -no-sql-mysql -no-sql-oci -no-sql-odbc -no-sql-psql -sql-sqlite -system-sqlite -sql-sqlite2 -no-sql-tds -nomake tests -make tools -no-tslib -libudev -widgets -no-xcb -system-zlib -skip webengine -c++std c++11 -skip qtdoc -qpa wayland
if [ "0" != "$?" ]; then
exit 1
fi
make
if [ "0" != "$?" ]; then
exit 1
fi
make install
if [ "0" != "$?" ]; then
exit 1
fi
cd ../$OUTPUT
tar -zcf ../qt-5.15.2-eglfs-wayland-build.tar.gz *
echo ====== SUCCESS ======
...
If everything is OK, you will get the built out binary Qt 5.15.2 in gzip file: qt-5.15.2-eglfs-wayland-build.tar.gz. The build process may take several hours.
It will coexist with Qt 5.6.3.
...