Overview
This page is for know issues and possible workarounds for RA MCU software, tools, and boards.
RA Known Issues
Issue 1
This is issue 1
Issue 2
This is issue 2and Workarounds
Here are some of the known RA/FSP issues and possible workarounds.
MCUboot Application in IAR Workbench
MCUboot is a secure bootloader for RA MCUs which includes a flash layout to enables the software update. The flash layout determines the flash size for the bootloader area and the primary/secondary image slot area. Renesas provides several MCUboot examples in e2studio. However, when in IAR Workbench, you will notice an error and have to follow additional steps to get your project building correctly. To see the detials, follow the link below.
Steps to Build MCUboot Application with IAR Workbench