...
RZ/A Supported Toolchains
- GNU ARM Embedded toolchain (GCC 6; 6-2016-q4-major ):
...
- Libgen for GNU ARM embedded toolchain (V1.2018.02 or higher version)
Cannot Debug RZ Application
Issue: After loading the Application code the debugger is unable to step through the code.
...
- All Applications that run from the Flash ( Serial Flash, Hyper, or Octa ) requires a bootloader to be loaded prior to loading the Application. The bootloader is responsible for configurating the RZA Flash interface and Flash chip. If the bootloader is not programmed the RZ will not operate correctly.
- Check that the boot mode switches are set to the correct Flash.
- Once the application is running press the Restart button ( NOT THE RESET ). This will engage the bootloader so the Flash is in the expected configuration. To automate this open the project Debug Configuration. Under the Debugger -> Connection Settings tab set the Connection -> Reset before Run. NOTE: If the application is running from RAM do not make this settings. By default the IDE turns this setting off.
J-Link Does not Work with IDE
Issue: The IDE GDB cannot find the JLink for hardware debugging.
...
- The Segger JLink for the the e2studio is installed with the IDE installation. If the IDE GDB cannot find the Jlink review the e2 studio Integrated Development Environment (User’s Manual: Getting Started Guide). Make sure the optional component Renesas RZ Debug Support is selected during installation.
Create C++Project
The Renesas RZ BSP, Driver, and Demo Application code is written C Code. To support a C++ project, a project needs to be created from scratch. The Following is the suggested method to create a project.
...