Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

IDE and other Tools

Please use separate e2studio for RA MCUs from RX/RL78/RH850 to avoid modifying toolchain any other development environment settings. e2studio for RA will include FSP, e2studio for other MCUs will include SC.

You may want to use a new dedicated Workspace if starting a big new project.

Long project file path is not recommended. Path names containing space or special characters may cause unexpected issue. It's a good practice that just create a "Workspace" folder as root directory and put project folders under the Workspace folder.

Update to latest SC, FSP, QE revisions might break the existing working project. Please seek Renesas technical help if you cannot figure out the reason, or you could reverse back to the old version. It is typically recommended you update to latest versions when start a new project and stay with these versions for this project.

Customer Motor Bring-up Procedure

Here are some key steps to bring up customer motor control using Renesas MCUs. Note this is just given as a typical example. It varies depending on actual applications. 

  1. Check Renesas website for related MCU motor control solution documents, algorithms, evaluation boards and kits, sample codes, etc.
  2. Requested motor control kit (MCK) for bench evaluation.
  3. Download the sample project code for the MCK, the related IDE and tools such as e2studio with FSP, Renesas Motor Workbench (RMW), etc.
  4. After successfully running the Renesas MCK, try connecting the customer motor with appropriate power supply if possible.
    1. Update the motor parameters, maximum RPM, maximum current, and other key parameters based on the actual application.
    2. Test the motor and perform tuning as necessary.
  5. Design customer board with maximum commonality to Renesas MCK boards to minimize FW changes.
  6. Develop customer FW based on Renesas sample code to work with the customer board.
  7. Bring up the customer system, perform tuning and testing.
  8. Reach out to Renesas sales and FAE, or online helps for any issues during the development.

RWM

Find the correct MAP to load

For successful communication from RMW, the correct RMT and MAP files need to be loaded into RMW.

For RX-family code, they are located in project Workspace, in project_name\app\rmw folder.

For RA-family code, they are located in project_name\src\application\user_interfacer\ics folder

In certain situations when the “copy” command in e2studio Post-build Steps is not working properly, the updated MAP file does not appear in the above-mentioned folder after compiling. In this case, you should be able to find the updated MAP in the folder given below to load into RMW.

For RX-family code, in project_name\HardwareDebug folder.

For RA-family code, in project_name\Debug folder.

Change a Linker File

Modify the “copy” command in e2studio Post-build Steps can copy the MAP file into the default rmw or ics folder automatically after compiling. Here is an example in RX code: xcopy /y ${ProjName}.map ..\app\rmw

Change RMW to communicate through VCOM port

Here is an example of the steps to change an object file for linker. how to change RMW to communicate through VCOM port, instead of using the communication board as default. 

In RA4T1 Tuner code, link need to do two things. 1. #define USE_BUILT_IN (1) and 2. Link "ICS2_RA4T1_Built_in.o" instead  instead of "ICS2_RA4T1.o" to allow RMW to communicate through VCOM port, instead of using the communication board.

Change the USE_BUILT_IN in r_mtr_ics.h file under src\application\user_interface\ics from default (0) to (1) as below.

Image Added

Find First find the Tool Settings in the Project Properties shown as below.  

Image Removed

Then change the object file in "Other objects" under GNU Arm Cross C Linker => Miscellaneous, from "ICS2_RA4T1.o" to "ICS2_RA4T1_Built_in.o". Click Apply and Close.

Image Added

Image Modified

Finally update the list under GNU Arm Cross C Linker, in "All options", replace "ICS2_RA4T1_Built_in.o" with "ICS2_RA4T1.o". Click Apply and Close.

Image Modified

Customer Motor Control Tuning Procedure

Here are some key steps to bring up motor control using Renesas MCUs. Note this is just given as a typical example. It varies depending on actual applications. 

  • Check Renesas website for related MCU motor control solution documents, algorithms, evaluation boards and kits, sample codes, etc.
  • Requested motor control kit (MCK) for bench evaluation.
  • Download the sample project code for the MCK, the related IDE and tools such as e2studio with FSP, Renesas Motor Workbench (RMW), etc.
  • After successfully running the Renesas MCK, try connecting the customer motor with appropriate power supply if possible.
    1. Update the motor parameters, maximum RPM, maximum current, and other key parameters based on the actual application.
    2. Test the motor and perform tuning as necessary.
  • Design customer board with maximum commonality to Renesas MCK boards to minimize FW changes.
  • Develop customer FW based on Renesas sample code to work with the customer board.
  • Bring up the customer system, perform tuning and testing.
  • Reach out to Renesas sales and FAE, or online helps for any issues during the development.

    Fastest RMW Update Rate

    If set to the maximum Baud Rate of each MCU, the fastest RMW update rate can be achieved at 50µs for all Renesas MCUs but one (RX13T). These two tables show the settings and maximum RMW update rate.

    RX Family

    MCU

    CPU Clock (MHz)

    Supply Clock (UART) (MHz)

    Baud Rate (Mbps)

    Max. Sampling Time (µs/4ch)

    Lib API (ics2_init) 4th argument char speed

    Lib API (ics2_init) 5th argument char mode

    RX72T

    200

    50

    6.25

    50

    0

    2

    RX66T

    160

    40

    5

    50

    0

    2

    RX26T

    120

    60

    7.5

    50

    0

    2

    RX24T

    80

    40

    5

    50

    0

    2

    RX23T

    40

    40

    5

    50

    0

    2

    RX13T

    32

    32

    1

    200

    3

    2

    RA Family

    MCU

    CPU Clock (MHz)

    Supply Clock (UART) (MHz)

    Baud Rate (Mbps)

    Max. Sampling Time (µs/4ch)

    Lib API (ics2_init) 3rd argument char speed

    Lib API (ics2_init) 4th argument char mode

    RA8T1

    480

    120

    10

    50

    1

    2

    RA6T3

    200

    100

    16.6

    50

    0

    2

    RA4T1

    100

    100

    16.6

    50

    0

    2

    RA6T2

    240

    120

    10

    50

    1

    2

    RA6T1

    120

    120

    15

    50

    0

    2

    As an example, in the case of RX66T, data can be displayed in as fast as 50µs with the following settings.

    < main.c, row 130>

    Before (default): ics2_init((void *)dtc_table, ICS_SCI6_PB0_PB1, ICS_INT_LEVEL,4,1);    /* initialize ics */

    After: ics2_init((void *)dtc_table, ICS_SCI6_PB0_PB1, ICS_INT_LEVEL,0,2);    /* initialize ics */

    <mtr_interrupt.c, row365-372>

    Before (default):

        /****** for ICS ******/

        g_u1_cnt_ics++;

        if (g_u1_cnt_ics >= 3)

        {

            g_u1_cnt_ics = 0;

            ics2_watchpoint(); /* call ICS */

        }

        /*********************/

     After:  Changed to call every cycle

        /****** for ICS ******/

        //g_u1_cnt_ics++;

        //if (g_u1_cnt_ics >= 3)

        //{

           // g_u1_cnt_ics = 0;

            ics2_watchpoint(); /* call ICS */

        //}

        /*********************/

    Motor Parameters

    Required Key Motor Parameters

    Correct motor parameters are important for achieving desired motor control performance, especially in FOC motor control. Please ensure the parameters on Motor Current Controller and Speed Controller are input correctly. If using sensorless control, also need to ensure the parameters in BEMF Observer are correct.

    The parameters can be provided by motor manufacture, identified by Renesas RMW Tuner, or measured manually. RWM User’s Manual describes Tuner function and usage. Section 10.8 of MCI-HV-1 APN describes the manual measurement method.   

    Here are the motor parameters needed for a BLDC motor: 

    Parameter

    Note

    Pole Pairs

    If motor spec gives the number of poles, need to divide it by 2.

    Resistance (ohm)

    This is resistance of one phase. If motor spec give line to line resistance, or measure from phase-to-phase resistance, need to divide the value by 2. 

    Inductance of d-axis (H)

    These two values will be same for PMSM motor but will be different (Lq > Ld) for IPMSM motor.

    If motor spec give line to line inductance, or measure from phase-to-phase inductance, need to divide the value by 2.

    Inductance of q-axis (H)

    Permanent magnetic flux (Wb)

    If motor spec gives BEMF constant (Ke in VkRPM), need to convert it to Flux. Flux = Ke/(2πf), where f is the electrical cycle frequency at 1000RPM

    (f = #Pole Pairs * 1000/60).

    Rotor inertia (kgm^2)

    Need to include load inertia also, not just the motor itself.

    Here are the motor parameters needed for an induction motor:

    Parameter

    Note

    Pole Pairs

    If motor spec gives the number of poles, need to divide it by 2.

    Stator Resistance (ohm)

    This is resistance of one phase of stator. If motor spec give line to line resistance, or measure from phase-to-phase resistance, need to divide the value by 2. 

    Rotor Resistance (ohm)

    This is resistance of one phase of rotor. If motor spec give line to line resistance, or measure from phase-to-phase resistance, need to divide the value by 2. 

    Mutual Inductance (H)This is the interaction inductance from one coil to another coil.
    Stator Leakage Inductance (H)This is the stator leakage inductance. 

    Rotor Leakage Inductance (H)

    This is the rotor leakage inductance.

    Input Motor Parameters

    To enter the correct motor parameters into the code, if using FSP, you can directly enter through FSP by selecting "Motor Speed Controller (rm_motor_speed)" and "Motor Current Controller (rm_motor_current)" (for FOC projects) and entering under Properties=> Settings=> Motor Parameter, as shown below. Remember to update in both places.

    Image Added

    Image Added

    Please also check the MTR_MOTOR_PARAMETER define in "r_mtr_motor_parameter.h". It is "0" as default and the motor parameters configured in FSP will be used. However, if it is "1", then the motor parameters configured in FSP will not be used. Instead, the motor parameters in the file "r_mtr_motor_parameter.h" will be used. 

    #define MTR_MOTOR_PARAMETER (0)

    In RX projects, you may directly update the parameters in "r_motor_targetmotor_cfg.h" file in motor_module/cfg, shown as below.

    Image Added  

    Motor Control Test and Tuning

    Handle Current Sensing Polarity

    Renesas MCI-LV inverter board has positive polarity on motor current sensing circuit, from shunt through amplifier to the ADC ports. Renesas sample software for MCI-LV inverter board is programmed for positive polarity. The current FSP versions also only support positive polarity.  

    When using an inverter board with negative polarity, the current detection polarity needs to be properly handled in the software. One example is using Renesas RAA227063 EVB, where gate driver IC’s internal current sense amplifiers have reversed polarity.  

    As an example, in RA family sensorless FOC motor control sample code, in the FSP generated code file "rm_motor_driver.c", there are negative signs in the phase current ADC readings as below. If you are using an inverter board with negative current sensing polarity, please remove these negative signs, AFTER using FSP to generate code.

       p_ctrl->f_iu_ad = -(f_addata[0]) * (p_extend_cfg->f_current_range / p_extend_cfg->f_ad_resolution);

       p_ctrl->f_iv_ad = -(f_addata[1]) * (p_extend_cfg->f_current_range / p_extend_cfg->f_ad_resolution);

       p_ctrl->f_iw_ad = -(f_addata[2]) * (p_extend_cfg->f_current_range / p_extend_cfg→f_ad_resolution);

    Adjust Maximum Speed

    To adjust the maximum motor rotating speed, for RA MCUs, change the “Maximum rotational speed (rpm)” of "Motor Speed Controller" in FSP.

    Image Added

    And also adjust the "Limit of over speed (rpm)" of "Motor Sensorless Vector Control (rm_motor_sensorless)" in FSP accordingly.

    Image Added

    In RX MCU code, change the following parameters settings of:

    #define MOTOR_CFG_MAX_SPEED_RPM (2400.0f) /* maximum speed [rpm] (mechanical angle) */ 

    #define SPEED_CFG_SPEED_LIMIT_RPM (2850.0f) /* over speed limit [rpm] (mechanical angle) */ 

    Adjust Speed Change Rate

    Normally slower speed changes will have better speed control, but too “sluggish” speed changes may not be acceptable in real application.

    To adjust motor speed change (acceleration and deceleration) rate, in RA code, modify “Step of speed climbing (rpm)” in Module Motor Speed Controller (rm_motor_speed) as shown below. The unit is rpm per speed control period (0.001 sec in below figure). This applies to both open-loop and close-loop speed control.  

    Image Added

    In RX code, change this parameter in the file "r_motor_module_cfg.h" under motor_module\cfg. The unit is rpm per second.

    #define SPEED_CFG_RATE_LIMIT_RPM (1000.0f)  /* Rate limit of speed change [rpm/s] */ 

    Suppress Vibration during Open Loop Period

    If observe motor control vibration during FOC Open Loop period, enable “Open-loop damping” in Motor Speed Controller could help.

    Image Added

    High Voltage Kit Testing

    When testing motor control kit with high voltage (such as 110V AC or 220V AC) and connecting your laptop, it is always safer to run the laptop on battery only. Do not connect external power supply or monitor. The goal is to let the laptop ground floating, even the communication interface is isolated.  

    Increase MCI-HV-1 Current Limit

    MCI-HV-1 high-voltage inverter board has a hardware peak current limit as 21.2A (INVERTER_CFG_CURRENT_LIMIT). With a safety margin of 2.0 (MOTOR_COMMON_CFG_OVERCURRENT_MARGIN_MULT, default setting is 2.0), the maximum allowed setting of motor phase RMS current as 7.5A (MOTOR_CFG_NOMINAL_CURRENT_RMS, default setting is 3.3A). If really want to use more current for motor, the safety margin could be reduced slightly, with minimum safe setting of 1.5. The maximum phase RMS current can then be increased to 10.0A with this minimum safety margin.

    Some Compiling Error Cases

    e2studio compiling error when using sinf, cosf functions

    If encounter compiling error when using sinf and cosf functions for trigonometric calculations, please go to the project properties, find "Settings" under "C/C++ Build". In "Tool Settings" tab, "Library Generator", "Standard Library", check the math.h (C89/C99), as shown in the figure below. Then click "Apply and Close", "Rebuild Index" and rebuild the code.

    Image Added

    e2studio compiling error when calling library functions

    If encounter compiling error when calling library functions, please make sure the library file is added to the Linker. As an example with RX26T, if the ics call functions such as ics_int_sci_rxi() is getting an error, please go to the project properties, find "Settings" under "C/C++ Build". In "Tool Settings" tab, "Linker", click the "Add file" button, select "Library" as the Format and find the "ICS2_RX26T.lib" in the "rmw" folder, as shown in the figure below. Then click "Apply and Close", "Rebuild Index" and rebuild the code.

    Image Added

    Troubleshoot Cases

    RZ/T & RZ/N CN032 AC Motor Control USB-Serial Driver issue

    For Windows 11, PC user will get driver error message when USB-Serial cable is connected. This is not seen in Windows 10 and previous versions as correct driver is automatically downloaded and installed by Windows. A way to work around this would be to remove/ uninstall the installed driver and locate previous 2019 version driver. Please contact AE team for driver, if needed.

    RA4T1 Tuner Issue

    Running RA4T1 sensorless FOC Tuner sample code with FSP 5.2.0 may get the error of "BSP_CFG_HANDLE_UNRECOVERABLE_ERROR(0);". It is because RA4T1 Tuner project needs a #define modification for this new FSP version. Making a correction on "AIDU_DEADTIME_SET" defined in "r_aid_tuner_gui_user.h" file as below will solve the issue.

    #define AIDU_DEADTIME_SET (g_user_motor_driver_extended_cfg.u2_deadtime) 

    MCI-HV-1 not Getting Boosted Bus Voltage of 390V DC

    When supply 100 V AC or 200 V AC 50 Hz power to the inverter, the bus voltage is automatically boosted to 390 V DC. If not getting the expected boosted bus voltage, please check below two things:

    1. Please make sure the jumpers JP7 and JP10 of MCU board MCB-RA6T2 are switched from default 2-3 pin short to 1-2 pin short.
    2. If the AC supply is at 60 Hz, please make the following changes.

    In file "r_pfc_cfg.h" under src\application\pfc_module\pfc\cfg folder, change

    VAC_FREQ from default (50.0f) to (60.0f)

    DATA_ARR_SIZE from default (320) to (267)

    Image Added


     

    Table of Contents