Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

  • RZ/G2 Series: RZ/G2L, RZ/G2LC, RZ/G2UL, RZ/G2E, RZ/G2N, RZ/G2M, RZ/G2H

  • RZ/G3 Series: RZ/G3S
  • RZ/V2 Series: RZ/V2L, RZ/V2M, RZ/V2MA

  • Verified Linux Package [5.10-CIP] Version 3.0.x
  •  Official RZ/G2 BSP Download Page
  •  Official RZ/V2 BSP Download Page
  • Please Download the individual components required for your MPU.
  • Please use the package versions listed table. You must match the correct component packages (Graphic, Codec) versions with the BSP version you are using.
.
VLP v3.0.4VLP v3.0.5-update3
Links
📦 RZ/G2 Linux Package (Common for all MPU    )
ZIP file containing Yocto BSP and all documentation
  • Yocto Recipe
    This is the actual BSP provided in a Yocto build package
  • Release Note for Linux Package
    Build instructions, start with this document
  • Reference Boards Linux Start-up Guide
    How to program the boot loaders into SPI flash
  • BSP Component list
    List of each package and version included in the default BSP build

RZ/G2


(works

,

not official)

RZ/

V2MA, RZ/V2M

G3 (all)
💾 Download Page


RZ/V2L, RZ/V2MA, RZ/

G2

V2M
💾 Download Page


RZ/

V2L
💾 Download Page

V2H
Contact Renesas

🎨 Graphics (PowerVR) and 🎦 Video Codec Libraries
  • For devices RZ/G2H, RZ/G2M, RZ/G2N, RZ/G2E
  • The "Evaluation Version" can be downloaded immediately, but has a 2 hour timeout after every board boot.
  • The "Unrestricted Version" request link is at the at the bottom of the download page (see Note1 below)
N/A

RZ/G2H, RZ/G2M, RZ/G2N, RZ/G2E

💾Multimedia Download Page

⚠️ See Note below for Fix (link) 

💾 Requires V1.0.2

🎨 Graphics (Mali) Libraries
  • For devices RZ/G2L, RZ/G2LC, RZ/V2L
  • The "Evaluation Version" can be downloaded immediately, but has a 2 hour timeout after every board boot.
  • The "Unrestricted Version" request link is at the at the bottom of the download page (see Note1 below)

RZ/G2L


(use V2L V1.1.0)
RZ/V2L
💾 Requires V1.1.0RZ/G2L
💾 Requires V1.1.2

, RZ/G2LC, RZ/G2UL
💾Download Page


RZ/V2L
💾 Download Page

🎦 Video Codec Libraries
  • For devices RZ/G2L and RZ/V2L
RZ/G2L
(use V2L V1.1.0)
💾Download Page

RZ/V2L
💾
 Requires V1.1.0RZ/G2L
💾 Requires V1.1.0
RZ/V2L
Download Page
🌐 HTML5 Browser (Gecko/Firefox)
  • For
devices RZ/G2L RZ/G2H, RZ/G2M, RZ/G2N, RZ/G2E🗨️ V2.0.3 (Gecko102)
  • devices some devices
💾 Download Page
📄 BSP Manual Set
Detailed information about Device Drivers and Device Tree Settings
📄 RZ/G2H, RZ/G2M, RZ/G2N, and RZ/G2E (link)

📄 RZ/G2L,RZ/G2LC, RZ/G2UL, RZ/V2L (link)

  • Note1 - Unrestricted Versions: When requesting the "Unrestricted Version", additional information about your product might be required. Additionally, but please allow up to 2 weeks for the request to complete due to internal license processing. When you submit a request, you will instantly get an email confirmation, but you will not get another email until the request has been completed.


Fix glibc Fetch Error During BSP Build

  • Affected BSP: All

Files were removed from the Debian server which causes a build error when building the BSP v3.0.6.

  • glibc_2.28-10+deb10u2.debian.tar.xz   (Removed from Server in May, 2024)
  • glibc_2.28-10+deb10u3.debian.tar.xz    (Removed form Server in July 2024)

This effects BSP v3.0.6, v3.0.6-update1, v3.0.6-update2

This issue has been fixed for v3.0.6-update3.

Below are instructions to download and apply patches to fix those issues for update1 or update 2.

cd meta-renesas
# Change deb10u2 to dev10u3
wget https://github.com/renesas-rz/meta-renesas/commit/a56169f6642d.patch
patch -p1 -i a56169f6642d.patch

# Change deb10u3 to dev10u4
wget https://github.com/renesas-rz/meta-renesas/commit/6c11ae542069.patch
patch -p1 -i 6c11ae542069.patch


RZ/G2 gstreamer1.0-omx-1.16.3-r0 do_fetch Error

  • Affected BSP: RZ/G2H, RZ/G2M, RZ/G2N, RZ/G2E

The Multimedia Package for RZ/G2 on renesas.com is V1.0.2

When building, the follow error will occur.

ERROR: gstreamer1.0-omx-1.16.3-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://anongit.freedesktop.org/gstreamer/common;destsuffix=git/common;name=common')

The reason is that the server name has change from anongit.freedesktop.org to gitlab.freedesktop.org

The easiest way to fix this issue is to run the command below from the base of your BSP directory.

sed -i 's/anongit/gitlab/' meta-rz-features/meta-rz-codecs/recipes-multimedia/gstreamer/gstreamer1.0-omx_1.16.3.bbappend


Linux Kernel 4.19 BSP

...