If you encounter any issues after the upgrade, please open a support request TICKET.🙌
Background
Some RX MCU peripherals use only fixed interrupt vectors, while some others also use software configurable interrupt vectors.
The software configurable interrupt vectors can configure select which interrupt is enable enabled by user depending on the applicationthe user. The software configurable interrupt is separated into two types for each clock source (PCKLA and PCLKB) as INTA and INTB.
It How to set the software configurable interrupt depends on which the driver is used if you use a software configurable interruptyou are using.
<p id="howToSet">
...
This is an example of how to remove the error for the GTCIU2 setting in GPT:
To resolve this error, you must configure additional interrupt settings in the "Interrupt Interrupts tab".
As shown in the figure below, you need to select the interrupt from the corresponding interrupt vector group, INTA or INTB.
Please also refer to the "User's Manual: Hardware" of each product to determine whether the interrupt belongs to INTA or INTB.(see also the appendix of this page)
...
The table for this information is shown in the following section:
Please check the r_bsp_interrupt_config.h located in the src/smc_gen/r_config/.
If the software configurable interrupt setting is not applied correctlysettings fails, the vector table may be set as blank.
Please check from this table in the Users manual: Hardware that you will use depens on if you faced this case, please handle the interrupt setting by using How to set the software configurable interrupt.