You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 12 Next »


SoC: All

Specification

Target Ubuntu OS Version: 20.04, 18.04

Target reference board: RZ/G2L,/G2LC,/G2UL SMARC

Host PC Environment: Ubuntu20.04

Ubuntu Filesystem Building

Install QEMU

Run below command on Host Ubuntu PC

sudo apt-get install qemu-user-static

Download Required Files


  • Download ubuntu-base-20.04.4-base-arm64

wget https://cdimage.ubuntu.com/ubuntu-base/releases/20.04/release/ubuntu-base-20.04.4-base-arm64.tar.gz

or

wget https://cdimage.ubuntu.com/ubuntu-base/releases/focal/release/ubuntu-base-20.04.4-base-arm64.tar.gz

  • Download ubuntu-base-18.04.5-base-arm64

wget http://cdimage.ubuntu.com/ubuntubase/releases/18.04.5/release/ubuntu-base-18.04.5-basearm64.tar.gz


Prepare Files

In the following example, please replace "version" as below name as you need

ubuntu-base-20.04.4-base-arm64: 20.04.4

ubuntu-base-18.04.5-base-arm64: 18.04.5


mkdir root

sudo tar -xpf ubuntu-base-<version>-base-arm64.tar.gz -C root

sudo cp /usr/bin/qemu-aarch64-static ./root/usr/bin/

sudo cp -b /etc/resolv.conf root/etc/resolv.conf

vim ch-mount.sh

#!/bin/bash function mnt() { echo "MOUNTING" sudo mount -t proc /proc ${2}proc sudo mount -t sysfs /sys ${2}sys sudo mount -o bind /dev ${2}dev sudo chroot ${2} } function umnt() { echo "UNMOUNTING" sudo umount ${2}proc sudo umount ${2}sys sudo umount ${2}dev } if [ "$1" == "-m" ] && [ -n "$2" ] ; then mnt $1 $2 elif [ "$1" == "-u" ] && [ -n "$2" ]; then umnt $1 $2 else echo "" echo "Either 1'st, 2'nd or both parameters were missing" echo "" echo "1'st parameter can be one of these: -m(mount) OR -u(umount)" echo "2'nd parameter is the full path of rootfs directory(with trailing '/')" echo "" echo "For example: ch-mount -m /media/sdcard/" echo "" echo 1st parameter : ${1} echo 2nd parameter : ${2} fi

Configure Filesystem

Enter Filesystem

chmod +x ch-mount.sh ./ch-mount.sh -m root/ chmod -R 777 /tmp

Install required software

apt-get update

apt-get install \ language-pack-en-base \ sudo \ ssh \ net-tools \ network-manager \ ethtool \ ifupdown \ isc-dhcp-client \ openssh-server \ iputils-ping \ rsyslog \ bash-completion \ htop \ resolvconf \ dialog \ vim

Add users

useradd -s '/bin/bash' -m -G adm,sudo <name>

passwd <name>

passwd root

chown -R root:root /bin/su

chmod u+s /bin/su


Configure UART

start on stopped rc or RUNLEVEL=[12345]

stop on RUNLEVEL [!12345]

respawn exec /sbin/getty -L 115200 ttyLP0 vt102


Network setup

echo "auto eth0" > /etc/network/interfaces.d/eth0 echo "iface eth0 inet dhcp" >> /etc/network/interfaces.d/eth0 echo "nameserver 8.8.8.8" >> /etc/resolv.conf echo "nameserver 8.8.4.4" >> /etc/resolv.conf

Exit FileSystem

exit ./ch-mount.sh -u root/

packaged FileSystem

cd root tar -cjf rootfs.tar.bz2 ./*

Deploy FileSystem to SD Card

Prepare a SD card with ext4 partition: SD Card Loading and Booting

extract ubuntu rootfs package to SD card

sudo tar -xvf rootfs.tar.gz -C /media/xxx/rootfs

Install Wayland, Wayland-Protocols and Weston

Environment Setup

  • sudo apt-get install pkg-config
  • sudo apt install ninja-build cmake git python3-pip kmod
  • sudo apt install libffi-dev libxml2 libxml2-dev graphviz doxygen xsltproc xmlto xdot libxkbcommon-dev libpixman-1-dev libinput-dev
  • sudo apt-get install libcairo-dev glib-2.0 libpango1.0-dev libjpeg-dev libwebp-dev libegl-mesa0 libsystemd-dev libgles2-mesa libgles2-mesa-dev libpam0g-dev libgbm-dev freerdp2-dev liblcms2-dev libx11-xcb-dev libcolord-dev libxcb-xkb1 libpipewire-0.2-dev libdbus-1-dev libxcb-xkb-dev libdrm-dev automake


Compile and install Wayland

Copy the Wayland 1.18.0 source code from VLP Yocto build folder to SD card home folder.

i.e. build/tmp/work/aarch64-poky-linux/wayland/1.18.0-r0/wayland-1.18.0/

  • export WLD=/usr

  • export LD_LIBRARY_PATH=$WLD/lib/aarch64-linux-gnu

  • export PKG_CONFIG_PATH=$WLD/lib/aarch64-linuxgnu/pkgconfig/:$WLD/share/pkgconfig/

  • export PATH=$WLD/bin:$PATH

  • sudo /root/.local/bin/meson build/ --prefix=$WLD \
    --libdir=$WLD/lib/aarch64-linux-gnu --sysconfdir=/etc

  • sudo ninja -C build/

  • sudo ninja -C build/ install

Compile and install Wayland-protocol

Copy the wayland-protocol1.20.0 source code from VLP Yocto build folder to SD card home folder.

i.e. build/tmp/work/aarch64-poky-linux/wayland-protocols/1.20-r0/wayland-protocols-1.20/
  • ./configure -- prefix=$WLD libdir=$WLD/lib/aarch64-linux-gnu

  • sudo make install

Compile and install Weston

Copy the weston8.0.0 source code from VLP Yocto build folder to SD card home folder.

i.e. build/tmp/work/aarch64-poky-linux/weston/8.0.0-r0/weston-8.0.0/
  • sudo /root/.local/bin/meson build/ --prefix=$WLD --libdir=$WLD/lib/aarch64-linux-gnu --sysconfdir=/etc -Dbackend-drm-screencast-vaapi=false -Dxwayland=false -Dcolor-management-colord=false -Dremoting=false


If the configuration is correct, it will display below messages

User defined options
    libdir : /usr/lib/aarch64-linux-gnu
    prefix : /usr
    sysconfdir : /etc
    backend-drm-screencast-vaapi : false
    color-management-colord : false
    remoting : false
    xwayland : false

Port GPU Libraries

Please refer to the StartupGuide.txt document in meta-rz-features/recipes-graphics/mali/files/mali_pkg_eval_vx.x.tar.gz

Migrate GPU drivers

Copy the driver mali_kbase..ko from VLP Yocto build folder to SD card.

i.e. build/tmp/work/smarc_rzg2l-poky-linux/kernel-modulemali/r35-p0/image/lib/modules/5.10.83-cip1-yocto-standard/extra
  • sudo insmod mali_kbase.ko

Migrate GPU Libraries

Copy the library files to SD card.

i.e.  meta-rz-features/recipesgraphics/mali/files/mali_pkg_eval_vx.x.tar.gz
Expandinstall library to reference board
  • tar -xf mali_um_r35p0.tar.gz
  • sudo cp -r mali_um/usr/lib/* /usr/lib/aarch64-linux-gnu/
  • sudo cp -r /usr/lib/aarch64-linux-gnu/CL_GLES/mali_wayland/

/usr/lib/aarch64-linux-gnu/

Testing

Install testing tool

sudo apt install glmark2-es2-wayland

Start Weston desktop

Only root user can launch weston service, please switch to root user in advance

insmod mali_kbase.ko
export XDG_RUNTIME_DIR=/usr/lib/
export RUNLEVEL=3
weston --tty 1 &

Run glmark2 test

glmark2-es2-wayland --fullscreen

glmark2 version

glmark2 result

Port codec Librasries

In this section, we will copy codec related files from original VLP Yocto build.

i.e. core-image-qt-smarc-rzg2l.tar.bz2 or core-image-weston-smarc-rzg2l.tar.bz2

Pleaes copy this .bz2 file to Ubuntu SD card and run below instruction on reference board

unzip core-image-qt-smarc-rzg2l.tar.bz2 or core-image-weston-smarc-rzg2l.tar.bz2 to folder "yocto"

copy codec drivers
  • cd ./yocto
  • mkdir /root/modules
  • cp lib/modules/5.10.83-cip1-yocto-standard/extra/* /root/modules/
copy gstreamer related lib
  • cp -rd usr/bin/gst-* /usr/bin/
  • cp -rd usr/lib64/libgst* /usr/lib/aarch64-linux-gnu/
  • cp -rd usr/lib64/gstreamer-1.0/ /usr/lib/aarch64-linux-gnu/
  • cp -rd usr/lib64/girepository-1.0/ /usr/lib/aarch64-linux-gnu/
  • cp -rd usr/lib64/libmmngr* /usr/lib/aarch64-linux-gnu/
  • cp -rd usr/lib64/libvspm.so.1* /usr/lib/aarch64-linux-gnu/
  • cp -rd usr/libexec/gstreamer-1.0/ /usr/lib/aarch64-linux-gnu/
  • cp -rd usr/share/gstreamer-1.0/ /usr/share/
  • cp -rd usr/share/gst-plugins-base/ /usr/share/
  • cp -rd usr/share/locale/en_GB/LC_MESSAGES/gst* /usr/share/locale/en_GB/LC_MESSAGES/
  • cp -rd usr/lib64/gstreamer-1.0/libgstomx.so /usr/lib/aarch64-linux-gnu/gstreamer-1.0/
  • cp -rd usr/lib64/libomxr_* /usr/lib/aarch64-linux-gnu/
  • cp -rd usr/lib64/libuvcs_* /usr/lib/aarch64-linux-gnu/
  • mkdir /lib64
  • cp -rd /usr/lib/aarch64-linux-gnu/ld-* /lib64/
  • cp etc/xdg/gstomx.conf /etc/xdg/
  • cp etc/gstpbfilter.conf /etc/
  • cp -r etc/omxr/ /etc/
modify omx plugin configuration
vi /etc/xdg/gstomx.conf

replace "lib64" as "lib/aarch64-linux-gnu"

[omxh264dec]
type-name=GstOMXH264Dec
core-name=/usr/lib/aarch64-linux-gnu/libomxr_core.so
component-name=OMX.RENESAS.VIDEO.DECODER.H264
·····
[omxh264enc]
type-name=GstOMXH264Enc
core-name=/usr/lib/aarch64-linux-gnu/libomxr_core.so
component-name=OMX.RENESAS.VIDEO.ENCODER.H264
···· 
install gstreamer dependency
apt install gstreamer1.0-libav gstreamer1.0-plugins-bad

Test gstreamer

login as root and insmod drivers
insmod /root/modules/mali_kbase.ko

insmod /root/modules/mmngr.ko

insmod /root/modules/mmngrbuf.ko

insmod /root/modules/uvcs_drv.ko

insmod /root/modules/vspm.ko

insmod /root/modules/vspm_if.ko


Specify gstreamer location
export GST_PLUGIN_SCANNER=/usr/lib/aarch64-linux-gnu/gstreamer-1.0/gst-plugin-scanner

export GST_PLUGIN_PATH=/usr/lib/aarch64-linux-gnu/gstreamer-1.0


Launch weston
weston –tty 1 &


Play Video
  • Play video only:

gst-launch-1.0 filesrc location=/root/video/sintel_trailer-720p.mp4 ! qtdemux ! queue ! h264parse ! omxh264dec ! waylandsink

  • Play video & audio

gst-launch-1.0 filesrc location=/root/video/sintel_trailer-720p.mp4 ! qtdemux name=d d. ! queue ! h264parse ! omxh264dec ! waylandsink d. ! queue ! faad ! alsasink device=plughw:0,0


Port Qt

You can port Qt by following 3 methods

  • Port from VLP
  • Compile & Install Qt from source
  • Install Qt by apt-get

Port from VLP

In this section, we will copy Qt5.6.3 related files from original VLP Yocto build.

i.e. core-image-qt-smarc-rzg2l.tar.bz2

Pleaes copy this .bz2 file to Ubuntu SD card and run below instruction on reference board

unzip core-image-qt-smarc-rzg2l.tar.bz2 to folder "yocto"

(For other version of Qt, you can modify Yocto meta-qt5\recipes-qt\qt5, please inqury Qt company for higher version QT integration)

Port Qt lib
cd yocto

cp -rd usr/share/qt5 /usr/share/

cp -rd usr/lib64/qt5 /usr/lib/aarch64-linux-gnu/

cp -rd usr/lib64/libQt* /usr/lib/aarch64-linux-gnu/

cp -rd usr/lib64/pkgconfig/Qt* /usr/lib/aarch64-linuxgnu/pkgconfig/

export QT_QPA_PLATFORM=wayland

export QT_PLUGIN_PATH=/usr/lib/aarch64-linux-gnu/qt5/plugins/


Start Weston RZ-G/RZ-G2 BSP Porting Ubuntu#Start Weston desktop

Then run the Qt example in /usr/share/qt5/examples

Compile from source

You can download qt5 source to reference board and compile on board.

Or cross compile qt5 on PC

Or compile qt5 in PC QEMU

Here we compile qt5 on board

Collapsecompile qt5
download qt5 source code by git (ignore)

mkdir qt5-build cd qt5-build make make install (rsync to SD)


We suggest to compile the qt5 with scrips

Notes: About the flags parameter in configure of Qt5. -qpa should be set as wayland or wayland-egl. We didn't support xcomposite-egl option

Install Qt by apt-get

apt-get install qt5-default qtwayland5

Notes: The above installation commands can only run part of Qt functions. If you need more functions, you need to continue installing Qt related packages.

Qt APPs development and testing

This section introduce how to develop Qt application on PC.

SDK build and installation

bitbake core-image-qt -c populate_sdk

The generated installation file is located at:

build/tmp/deploy/sdk/poky-glibc-x86_64-core-image-qtaarch64-smarc-rzg2l-toolchain-3.1.14.sh

Install this SDK to PC, default folder is /opt/poky/3.1.14

setup SDK runtime environment

source /opt/poky/3.1.14/environment-setup-aarch64-poky-linux 

QT creator configuration

Add Device

Add new Kit

Add Qt version

Add compiler

Add debuggers

Select kit to build Qt project

example to run qt calculator project


  • No labels