🎩🐇🃏🔮

This page contains many helpful suggestions for debugging issues with the Linux kernel.


Common Tools

  • grep : The kernel has thousands of files. The grep tool is the most powerful way to find what you are looking for. Use the -R to search recursively . Remember that grep is case sensitive by default, so use -i if you need it to ignore case.
    • And example to find a function name start_kernel: $ grep -r "start_kernel"
  • find : Sometimes someone will give you just a filename, and the find command can help you find where that file is. Also, it find is very helpful when combined with grep.
    • For example, if you just want to search header files: $ find * -name "*.h" | grep purple
  • printf / printk : Believe it or not, printf and printk are still the most used debug methods for kernel developers. It's simple, and works on any system. For the kernel, the printf function is called printk. But if you are debugging something like u-boot, you will the standard printf

Error Messages

  • Many times an error message will be printed out. This happens a lot for a device driver that has trouble initializing during boot.
  • Your first step should be to find what source code file is print that message
  • Simply use the grep command with -R option and search for that error message.

Error Codes

  • If a error message prints out an error code, for example "-110", you should look up what the error code means.
  • You can find a list of the error code numbers mean in file include/uapi/asm-generic/errno-base.h
  • Since the code will use the #defrine name (not the actual number), you can then search driver file for when that error code/name is returned.

Finding the Device Driver File

  • When adding or configuring a driver to your system, you will probably be editing the Device Tree.
  • If there is an issue with that driver or peripheral, you will need to find the source code for the driver
  • You can use the "compatible" name listed in the device tree, and grep, in order to find the location of the device driver file.
  • Do you search starting in the "drivers" directory (to avoid all the matches that will be found in other device tree files)
  • Example: Find the Watchdog Timer Driver
    • RZ/G2L Device Tree: rz_linux-cip/arch/arm64/boot/dts/renesas/r9a07g044.dtsi
      wdt0: watchdog@12800800 {
      	compatible = "renesas,r9a07g044-wdt",
      		     "renesas,rzg2l-wdt";
      	reg = <0 0x12800800 0 0x400>;
      	clocks = <&cpg CPG_MOD R9A07G044_WDT0_PCLK>,
      		 <&cpg CPG_MOD R9A07G044_WDT0_CLK>;
      	clock-names = "pclk", "oscclk";
      	interrupts = <GIC_SPI 49 IRQ_TYPE_LEVEL_HIGH>,
      		     <GIC_SPI 50 IRQ_TYPE_LEVEL_HIGH>;
      	interrupt-names = "wdt", "perrout";
      	resets = <&cpg R9A07G044_WDT0_PRESETN>;
      	power-domains = <&cpg>;
      	status = "disabled";
      };
      
    • Use the grep command:
      $ grep -R "renesas,rzg2l-wdt" *
      arch/arm64/boot/dts/renesas/r9a07g044.dtsi:				     "renesas,rzg2l-wdt";
      arch/arm64/boot/dts/renesas/r9a07g044.dtsi:				     "renesas,rzg2l-wdt";
      arch/arm64/boot/dts/renesas/r9a07g044.dtsi:				     "renesas,rzg2l-wdt";
      arch/arm64/boot/dts/renesas/r9a07g043.dtsi:				     "renesas,rzg2l-wdt";
      arch/arm64/boot/dts/renesas/r9a07g043.dtsi:				     "renesas,rzg2l-wdt";
      arch/arm64/boot/dts/renesas/r9a07g054.dtsi:				     "renesas,rzg2l-wdt";
      arch/arm64/boot/dts/renesas/r9a07g054.dtsi:				     "renesas,rzg2l-wdt";
      arch/arm64/boot/dts/renesas/r9a07g054.dtsi:				     "renesas,rzg2l-wdt";
      Documentation/devicetree/bindings/watchdog/renesas,wdt.yaml:          - const: renesas,rzg2l-wdt     # RZ/G2L
      Documentation/devicetree/bindings/watchdog/renesas,wdt.yaml:              - renesas,rzg2l-wdt
      drivers/watchdog/rzg2l_wdt.c:	{ .compatible = "renesas,rzg2l-wdt", },
      scripts/dtc/include-prefixes/arm64/renesas/r9a07g044.dtsi:				     "renesas,rzg2l-wdt";
      scripts/dtc/include-prefixes/arm64/renesas/r9a07g044.dtsi:				     "renesas,rzg2l-wdt";
      scripts/dtc/include-prefixes/arm64/renesas/r9a07g044.dtsi:				     "renesas,rzg2l-wdt";
      scripts/dtc/include-prefixes/arm64/renesas/r9a07g043.dtsi:				     "renesas,rzg2l-wdt";
      scripts/dtc/include-prefixes/arm64/renesas/r9a07g043.dtsi:				     "renesas,rzg2l-wdt";
      scripts/dtc/include-prefixes/arm64/renesas/r9a07g054.dtsi:				     "renesas,rzg2l-wdt";
      scripts/dtc/include-prefixes/arm64/renesas/r9a07g054.dtsi:				     "renesas,rzg2l-wdt";
      scripts/dtc/include-prefixes/arm64/renesas/r9a07g054.dtsi:				     "renesas,rzg2l-wdt";
      
    • The very bottom of file drivers/watchdog/rzg2l_wdt.c
      static const struct of_device_id rzg2l_wdt_ids[] = {
      	{ .compatible = "renesas,rzg2l-wdt", },
      	{ /* sentinel */ }
      };
      MODULE_DEVICE_TABLE(of, rzg2l_wdt_ids);
      
      static struct platform_driver rzg2l_wdt_driver = {
      	.driver = {
      		.name = "rzg2l_wdt",
      		.of_match_table = rzg2l_wdt_ids,
      	},
      	.probe = rzg2l_wdt_probe,
      };
      module_platform_driver(rzg2l_wdt_driver);
      
      MODULE_DESCRIPTION("Renesas RZ/G2L WDT Watchdog Driver");
      MODULE_AUTHOR("Biju Das ");
      MODULE_LICENSE("GPL v2");
      


View Interrupts

  • The 'virtual' file /proc/interrupts lists every interrupt in the system, and counts every time an that interrupt occurs.
  • Use this command to print it out
$ cat /proc/interrupts
  • When a device is not working, first check if interrupts are occurring and that will tell you a lot. This is usually the first step in any debugging.
  • Sometime device operations will fail silently (no error message), but if you see an interrupt occurred, you can at least know something has happened.
  • For example, maybe you are trying to detect an I2C device on boot up, but you do not see any message for it. If you check for I2C controller interrupts, then you at least know the I2C works, but maybe it's not using the correct I2C address. This means there is no "error" to report (other than you make a mistake in your Device Tree).


Nothing prints after message "Starting kernel..."

Sometimes you might have a case were u-boot loads the kernel image and device tree, but when you start to boot the kernel, nothing happens. The last message you see is "Starting kernel..."

For example:

Hit any key to stop autoboot: 0 
19843584 bytes read in 827 ms (22.9 MiB/s)
59411 bytes read in 6 ms (9.4 MiB/s)
Moving Image from 0x48080000 to 0x48200000, end=49560000
## Flattened Device Tree blob at 48000000
Booting using the fdt blob at 0x48000000
Using Device Tree in place at 0000000048000000, end 0000000048011812
Starting kernel ...


The reason is that the kernel will start to run, but something makes it crash before the serial console is configured. So, you will never get to see the error messages. For example, if you have a mistake in your device tree for the memory configuration, the system will crash early before the serial console driver is loaded.

However, there is a way for your to print out those early messages. You can tell the kernel to continue to use the same serial connection that u-boot used since it is already configured and working. To use that serial port peripheral, the kernel only needs a very simple driver where each serial characters is sent out one at a time since there will not be any interrupts set up yet. This driver is already support for all the RZ devices.

This feature is called earlycon

To enable, add earlycon to your kernel boot arguments to print out the error messages.

=> setenv bootargs 'root=/dev/mmcblk1p2 rootwait earlycon'
=> booti 0x48080000 - 0x48000000'

Then, you will at least see some text come out that might be helpful to you.

Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd073]
[ 0.000000] Linux version 5.10.184-cip36-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 8.3.0, GNU ld (GNU Binutils) 2.31.1) #1 SMP PREEMPT Tue Apr 5 23:00:00 UTC 2011
[ 0.000000] Machine model: HopeRun HiHope RZ/G2N with sub board
[ 0.000000] earlycon: scif0 at MMIO 0x00000000e6e88000 (options '115200n8')
[ 0.000000] printk: bootconsole [scif0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000058000000, size 512 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma@58000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000078000000, size 256 MiB
[ 0.000000] OF: reserved mem: initialized node linux,multimedia@70000000, compatible id shared-dma-pool

If there are no Error Messages

  • Sometimes you get clues that the driver might be doing something (interrupts), but not really sure what or why. In that case, you can put some print message in the API calls into the driver.

For example, say that the system was saying it was playing audio, but nothing was coming out. Basically if aplay works and you don't see anything, then it's 1 of 2 issues:

1. The pins are not really configured correctly

2. You have the channel muted so the alsa subsystem doesn't even bother sending data to the driver.

The driver is sound/soc/sh/rz-rssi.c

The way alsa drivers work is, first configures the audio for the correct sample rate, then it breaks the data up into blocks and feeds them one at a time. Basically, here are the APIs:

 
static const struct snd_soc_dai_ops rz_ssi_dai_ops = {
        .trigger        = rz_ssi_dai_trigger,
        .set_fmt        = rz_ssi_dai_set_fmt,
        .hw_params        = rz_ssi_dai_hw_params,
};

The function rz_ssi_dai_trigger() is the one that the audio subsystems calls over an over again with blocks of data to send out.

By putting a printk in that function to see if it is really getting called or not.

That will at least point you in a direction to look next.

How to read a Crash Log

There are many different situations that may lead to a kernel panic, the one below is an example:

root@smarc-rzg2ul:~# mount -t nfs 192.168.10.118:/home/micbis/renesas/repos/vlp3/build/tmp/deploy/images/smarc-rzg2ul /mnt 
root@smarc-rzg2ul:~# cp /mnt/core-image-weston-smarc-rzg2ul-20221207082338.rootfs.ext4 .

[   40.178861] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000402
[   40.187626] Mem abort info:
[   40.190404]   ESR = 0x96000004
[   40.193443]   EC = 0x25: DABT (current EL), IL = 32 bits
[   40.198727]   SET = 0, FnV = 0
[   40.201763]   EA = 0, S1PTW = 0
[   40.204885] Data abort info:
[   40.207748]   ISV = 0, ISS = 0x00000004
[   40.211562]   CM = 0, WnR = 0
[   40.214514] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000055024000
[   40.220921] [0000000000000402] pgd=0000000000000000, p4d=0000000000000000
[   40.227683] Internal error: Oops: 96000004 [#1] PREEMPT SMP
[   40.233227] Modules linked in: vspm_if(O) vspm(O) mmngrbuf(O) mmngr(O)
[   40.239745] CPU: 0 PID: 237 Comm: cp Tainted: G           O      5.10.131-cip13-yocto-standard #1
[   40.248571] Hardware name: Evaluation board based on r9a07g043u11 (DT)
[   40.255066] pstate: 00400085 (nzcv daIf +PAN -UAO -TCO BTYPE=--)
[   40.261056] pc : ___slab_alloc.constprop.105+0x58/0x6f8
[   40.266255] lr : ___slab_alloc.constprop.105+0x61c/0x6f8
[   40.271538] sp : ffff80001a46b690
[   40.274833] x29: ffff80001a46b690 x28: ffff80001a46bc58
[   40.280122] x27: ffff000009413d00 x26: ffff00007fc10920
[   40.285410] x25: 0000000000000000 x24: ffff800011059000
[   40.290699] x23: 000000000007abf8 x22: 0000000000000dc0
[   40.295987] x21: 0000000000000dc0 x20: fffffe000009edc0
[   40.301276] x19: ffff800010da0c18 x18: 00000000000000c0
[   40.306564] x17: 0000000000000010 x16: 0000000000000000
[   40.311852] x15: 0000000000000001 x14: 0000000000000003
[   40.317140] x13: 000000000004ff76 x12: dead000000000122
[   40.322428] x11: 0000000000000000 x10: ffff00000f521400
[   40.327716] x9 : 000000000000000e x8 : 0000000000000001
[   40.333005] x7 : ffff80006ed13000 x6 : ffff800011190000
[   40.338292] x5 : 0000000000440000 x4 : fffffe000009ee20
[   40.343581] x3 : 0000000000000403 x2 : 000000000006c808
[   40.348869] x1 : 0000000000000403 x0 : 0000000000000402
[   40.354159] Call trace:
[   40.356595]  ___slab_alloc.constprop.105+0x58/0x6f8
[   40.361450]  __slab_alloc.isra.96.constprop.104+0x2c/0x58
[   40.366822]  kmem_cache_alloc+0x2d0/0x2f0
[   40.370814]  __nfs_create_request.part.20+0x58/0x190
[   40.375754]  nfs_create_request+0x7c/0xa0
[   40.379744]  readpage_async_filler+0x21c/0x250
[   40.384168]  read_cache_pages+0xcc/0x198
[   40.388071]  nfs_readpages+0xec/0x1f8
[   40.391714]  read_pages+0x188/0x288
[   40.395186]  page_cache_ra_unbounded+0x140/0x218
[   40.399779]  do_page_cache_ra+0x40/0x50
[   40.403596]  ondemand_readahead+0x128/0x2d0
[   40.407758]  page_cache_async_ra+0xe0/0xe8
[   40.411833]  generic_file_buffered_read+0x17c/0x9c8
[   40.416686]  generic_file_read_iter+0x100/0x1a0
[   40.421193]  nfs_file_read+0x78/0x100
[   40.424839]  new_sync_read+0x104/0x180
[   40.428569]  vfs_read+0x148/0x1d0
[   40.431866]  ksys_read+0x68/0xf0
[   40.435077]  __arm64_sys_read+0x1c/0x28
[   40.438897]  el0_svc_common.constprop.4+0x8c/0x180
[   40.443663]  do_el0_svc+0x24/0x90
[   40.446963]  el0_svc+0x14/0x20
[   40.450000]  el0_sync_handler+0x90/0xb8
[   40.453817]  el0_sync+0x160/0x180
[   40.457120] Code: f9400681 d1000420 f240003f 9a941000 (f9400000)
[   40.463186] ---[ end trace e6200b448c7a9881 ]---

Here's a breakdown of some key information in the first part of the log:

  • Unable to handle kernel NULL pointer dereference: This indicates that the kernel attempted to access or dereference a NULL pointer, which often leads to a crash.
  • virtual address 0000000000000402: Specifies the virtual address where the NULL pointer dereference occurred.
  • Mem abort info: Provides additional information about the memory abort.
    • ESR = 0x96000004: The Exception Syndrome Register (ESR) value. The raw hex value is then decoded:
      • EC = 0x25: DABT (current EL), IL = 32 bits
      • SET = 0, FnV = 0
      • EA = 0, S1PTW = 0

The important bit is that it was a data abort at the current Exception Level (so the kernel itself).

  • Data abort info: Gives details about the data abort, including Information Syndrome (ISV), Instruction Syndrome (ISS), etc.
    • ISV = 0, ISS = 0x00000004
    • CM = 0, WnR = 0

In this specific case, it was a read (WnR = 0), not a cache maintenance instruction (CM = 0), the Instruction Syndrome was not valid (ISV = 0) and ISS = 0x4 means Translation fault, level 0.

  • user pgtable: Describes the user page table characteristics, i.e. more information about the MMU and related configuration.
    • user pgtable: 4k pages, 48-bit VAs, pgdp=0000000055024000: Specific information about page table configuration in the system

[0000000000000402] pgd=0000000000000000, p4d=0000000000000000: Specific information about the page global directory and page table entries.

Unless you are really developing the kernel, this is not usually very important.

Overall, by reading this first part of the log we can deduce that it was a problem probably related to memory, some wrong access due to something.

Continuing with the breakdown:

  • Internal error: Oops: 96000004 [#1] PREEMPT SMP: Indicates an internal error, often referred to as an "Oops," with error code 96000004. The system is preemptible, symmetric multiprocessing (SMP) is enabled, and this is the first Oops encountered (#1).
  • Modules linked in: Lists the kernel modules that are loaded. In this case, it includes modules like vspm_if, vspm, mmngrbuf, and mmngr.
  • CPU: 0 PID: 237 Comm: cp Tainted: G O 5.10.131-cip13-yocto-standard #1: Provides information about the CPU, process ID (PID), command (Comm), and kernel version. The system is marked as "Tainted," which might indicate that non-GPL (General Public License) or proprietary modules are loaded.
  • Hardware name: Evaluation board based on r9a07g043u11 (DT): Specifies the hardware platform, in this case the RZ/G2UL.
  • pc : ___slab_alloc.constprop.105+0x58/0x6f8: Indicates the program counter value at the time of the crash, pointing to the function ___slab_alloc.constprop.105.
  • lr : ___slab_alloc.constprop.105+0x61c/0x6f8: Shows the link register value.
  • Registers (x29, x28, ..., x0): Display the values of various registers at the time of the crash.

By far the most important part is the program counter. It tells us which function caused the crash, from the name we can deduce it was a specific type of malloc, consistent with the data abort previously signaled (more information in the call stack). The stack pointer (sp) may often give other hints. From the registers dump you can notice that many registers holds 64-bit values beginning with 0xffff, this is expected because this is the kernel address space, in contrast with user-space (0x0). What you may want to check is whether some registers hold weird 64-bit values, this is often an indication of something wrong. x0 is also something you may want to monitor closely: in the Arm64 Procedure Call Standard it is used to pass the first function parameter and for the return value.

The last part is the call stack. We can retrieve some useful information from it. Starting from the bottom:

  • el0_svc+0x14/0x20: This suggests that the crash was caused by some user-space (exception level 0 service call) application. In this case it was a copy from / to the network.
  • nfs_file_read+0x78/0x100: Again indication about nfs related business.
  • kmem_cache_alloc+0x2d0/0x2f0: Some kernel memory cache allocation that finally ended with the data abort.

To conclude, in this specific case this kernel crash was triggered by a innocuous network copy, experienced during the BSP porting on a custom board. We can reasonably exclude (at least initially) a kernel bug, so what we may want to look into is everything that may be related to memory. Eventually this was due to a silly mistake in the memory section of the device tree: 2GB defined whereas the custom board implemented 1GB only. Note that this may not be immediately visible, it occurred only when the kernel tried to allocate something in the non-existing gigabyte.

Force a Stack Trace Dump

  • There are many ‘soft pointers’ in the kernel, so sometimes you can’t figure how you got into a function. You get a warning message, and you know what file printed the message, but you cannot figure out "who" called that function.
  • The WARN_ON(1) macro defined by the kernel will cause a stack dump so you can see who called that function. Since it is a Warning macro it will not cause the system to crash. The system ill continue to operate.
  • You can also put some condition in WARN_ON. For example: WARN_ON( my_flag == 1);
  • There is also a WARN_ONCE( ) macro that will make the stack dump only print once.
  • There is an example where there is an argument passed to function rzg2l_mip_dsi_attached() that causes an error (maybe from a bad Device Tree value). But, you need to know what function called it. The issue is that is determined at run-time, not compiled time. So by using the WARN_ON macro, you can get the call trace. Since the next step would be to print out some debug info (using printk) in the calling function, the WARN_ON(1) will print out the call trace so you will know what function that was. Then, you can use 'grep' to find what file has that function.
[    2.039546] Call trace:
[    2.041986]  rzg2l_mipi_dsi_attach+0x5c/0x244  <<< Where we put our WARN_ON
[    2.046336]  drm_bridge_attach+0x64/0xc4       <<< Where we need to look next for the bad args 
[    2.050254]  rcar_du_encoder_init+0xac/0x140
[    2.054514]  rcar_du_modeset_init+0x3b4/0x4ac
[    2.058861]  rcar_du_probe+0xb0/0x16c
[    2.062514]  platform_drv_probe+0x50/0xa0
[    2.066515]  really_probe+0x260/0x3d0
[    2.070169]  driver_probe_device+0x54/0xf0     <<< Means this is all part of the initial driver loading at boot time
[    2.074256]  __device_attach_driver+0xc0/0x110
[    2.078689]  bus_for_each_drv+0x78/0xd0
[    2.082516]  __device_attach+0xd8/0x174
[    2.086344]  device_initial_probe+0x10/0x20
[    2.090517]  bus_probe_device+0x90/0xa0
[    2.094344]  deferred_probe_work_func+0x6c/0xa0
[    2.098867]  process_one_work+0x1b8/0x304
[    2.102867]  worker_thread+0x23c/0x44c
[    2.106607]  kthread+0x128/0x160
[    2.109829]  ret_from_fork+0x10/0x1c

Bind and Unbind Drivers

  • If you want to completely reset a peripheral, you can 'unbind' the device from the driver, then 'bind' it back again.
  • When you bind, it is the same operation that happened during system boot (setup up the register, reads the settings from the Device Tree, looks for attached devices, etc...)
  • Here is an old article by Greg K-H, but still relevant today: https://lwn.net/Articles/143397/

Using initcall_debug

  • The use of initcall_debug is good to confirm that your driver is being loaded on boot.
  • When you are not seeing your device show up in the system, you should check your boot log to see if there are any error messages from the driver.
  • If you do not see any message at all from the driver, you might want to make sure your driver is being loaded. To do that, you will want to add initcall_debug to the kernel command line.
  • For example, in u-boot:
=> setenv bootargs 'root=/dev/mmcblk1p2 rootwait initcall_debug'
=> booti 0x48080000 - 0x48000000'
  • The initcall_debug option will make the kernel print out every driver it has loaded in the system. Expect to see a lot of text. However, you can then check that log to make sure your driver was loaded.
  • If you do not see your driver being loaded, it might not be enabled in the kernel (menuconfig).
  • Drivers vs Devices: Remember, during kernel boot, the kernel initializes each driver one at a time. And after each driver initialization, the kernel then checks the Device Tree to see if any devices are declared. That is what the "compatible" string is used for.....drivers and devices to be matched up by string name (a simple string compare). If a device's 'compatible' (in the Device Tree) name matches a driver 'compatible' name (in the kernel driver), then the kernel will immediately call the "probe" function inside the driver code in order to try and detect, set up and configure that driver. If a driver is loaded (you see the init() function in the driver called), but the probe() function in the driver is not called (you can put a printk message to confirm), then the kernel did not find a matching compatible string.

Debugfs

In the Linux Kernel, many drivers and subsystems have support for a special file system called debugfs. This special file system is enabled and mounted by default with VLP:

mount
/dev/mmcblk0p6 on / type ext4 (rw,relatime)
[...]
debugfs on /sys/kernel/debug type debugfs (rw,nosuid,nodev,noexec,relatime)
[...]

As usual you can use the cat command to view the content of this file system. For example clock:

cat /sys/kernel/debug/clk/clk_summary
                                 enable  prepare  protect                                duty
   clock                          count    count    count        rate   accuracy phase  cycle
---------------------------------------------------------------------------------------------
 32k                                  0        0        0       32768          0     0  50000
 x1-clock                             4        4        0    24000000          0     0  50000
    ref                               1        1        0    24000000          0     0  50000
    pfd1                              1        1        0    24000000          0     0  50000
       pll1                           2        2        0   600000000          0     0  50000
          div2                        1        1        0    12000000          0     0  50000
             se3_mux                  1        1        0    12000000          0     0  50000
                se3                   1        1        0    12000000          0     0  50000
          div1_mux                    1        1        0   600000000          0     0  50000
             div1                     1        1        0    25000000          0     0  50000
                diff1_mux             1        1        0    25000000          0     0  50000
                   diff1              1        1        0    25000000          0     0  50000
    pfd3_mux                          1        1        0    24000000          0     0  50000
       pfd3                           1        1        0      960000          0     0  50000
          pll3                        1        1        0   564480000          0     0  50000
             div5                     2        2        0    11289600          0     0  50000
                se1_mux               1        1        0    11289600          0     0  50000

[...]

GPIO:

cat /sys/kernel/debug/gpio
gpiochip0: GPIOs 120-511, parent: platform/11030000.pinctrl, 11030000.pinctrl:
 gpio-120 (P0_0                )
 gpio-121 (P0_1                )
 gpio-122 (P0_2                )
 [...]
 gpio-149 (P3_5                )
 gpio-150 (P3_6                )
 gpio-151 (P3_7                )
 gpio-152 (P4_0                )
 gpio-153 (P4_1                |gpio_sd0_pwr_en     ) out hi
 gpio-154 (P4_2                )
 [...]

Pin muxing:

root@smarc-rzg2l:~# cat /sys/kernel/debug/pinctrl/11030000.pinctrl-pinctrl-rzg2l/pinmux-pins
Pinmux settings per pin
Format: pin (name): mux_owner|gpio_owner (strict) hog?
pin 0 (P0_0): UNCLAIMED
pin 1 (P0_1): UNCLAIMED
pin 2 (P0_2): UNCLAIMED
pin 3 (P0_3): UNCLAIMED
[...]
pin 30 (P3_6): UNCLAIMED
pin 31 (P3_7): UNCLAIMED
pin 32 (P4_0): device 11c50200.usb-phy function usb0 group usb0
pin 33 (P4_1): GPIO 11030000.pinctrl:153
pin 34 (P4_2): UNCLAIMED
pin 35 (P4_3): UNCLAIMED
pin 36 (P4_4): UNCLAIMED
pin 37 (P4_5): UNCLAIMED
pin 38 (P4_6): UNCLAIMED
pin 39 (P4_7): UNCLAIMED
pin 40 (P5_0): device 11c50200.usb-phy function usb0 group usb0
pin 41 (P5_1): device 11c50200.usb-phy function usb0 group usb0
pin 42 (P5_2): UNCLAIMED
pin 43 (P5_3): UNCLAIMED
pin 44 (P5_4): UNCLAIMED
pin 45 (P5_5): UNCLAIMED
[...]
pin 68 (P8_4): UNCLAIMED
pin 69 (P8_5): UNCLAIMED
pin 70 (P8_6): UNCLAIMED
pin 71 (P8_7): UNCLAIMED
pin 72 (P9_0): device 10059000.adc function adc group adc
[...]

DRI:

cat /sys/kernel/debug/dri/0/state
plane[32]: plane-0
        crtc=crtc-0
        fb=46
                allocated by = weston
                refcount=2
                format=XR24 little-endian (0x34325258)
                modifier=0x0
                size=1920x1080
                layers:
                        size[0]=1920x1080
                        pitch[0]=7680
                        offset[0]=0
                        obj[0]:
                                name=0
                                refcount=3
                                start=00100384
                                size=8294400
                                imported=no
                                paddr=0x0000000058600000
                                vaddr=00000000fcba5467
        crtc-pos=1920x1080+0+0
        src-pos=1920.000000x1080.000000+0.000000+0.000000
        rotation=1
        normalized-zpos=0
        color-encoding=ITU-R BT.601 YCbCr
        color-range=YCbCr limited range
plane[34]: plane-1
        crtc=(null)
        fb=0
        crtc-pos=0x0+0+0
        src-pos=0.000000x0.000000+0.000000+0.000000
        rotation=1
        normalized-zpos=0
        color-encoding=ITU-R BT.601 YCbCr
        color-range=YCbCr limited range
crtc[37]: crtc-0
        enable=1
        active=1
        self_refresh_active=0
        planes_changed=0
        mode_changed=0
        active_changed=0
        connectors_changed=0
        color_mgmt_changed=0
        plane_mask=1
        connector_mask=1
        encoder_mask=1
        mode: "1920x1080": 60 148500 1920 2008 2052 2200 1080 1084 1089 1125 0x48 0x5
connector[39]: HDMI-A-1
        crtc=crtc-0
        self_refresh_aware=0
        max_requested_bpc=0
connector[45]: Writeback-1
        crtc=(null)
        self_refresh_aware=0
        max_requested_bpc=0

But there are much more useful information that can be found in there and of course you can use grep command to filter the output.

  • No labels