There've been multiple support requests regarding the discontinued support for VDPA configuration. Currently customers are instructed to modify bytes in a binary file to be able to configure that.
To improve quality of support a Python script shall be created which:
VDPARead_Update.py and NSC_RF_CONFIG.dat should be at same location
user should execute commandÂ
python VDPARead_Update.py NSC_RF_CONFIG.dat
Â
after execution user would be asked to enter VDPA value to be updated.
after successful update, VDPA update successful
 message will be printed.
this script is valid for .dat file versions 0x06,0x08,0x0A and 0x0C