You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 14 Next »

Overview

This page is for quick tips to help you with RL78 MCUs, its software, tools, and boards.  If you have any tips, please let us know and we will include them here.  

RL78 Tips and Tricks

Here are the frequently asked RL78 questions and answers to them.  There are a few tips and tricks also to help your journey with your development.  

What is Self RAM for RL78 MCUs?

In RL78 series MCUs, "Self RAM" refers to the RAM area that must be allocated or reserved when the user utilizes the RL78 series Flash Self-Programming Library.

The relevant application documentation for the RL78 series Flash Self-Programming Library includes descriptions of Self RAM. For example, the section 9.4 "Defining the Internal RAM Area" in the RL78 Family Flash Self-Programming Library Type01 Package Ver.4.00 Release Note provides detailed information about Self RAM allocation.

See more...

How can a binary file exceeding 64KB be linked to code flash when developing with CC-RL?

The description in one Knowledge Base article states that with the use of the -binary option in Linker, binary files within 64KB can be assigned to the address range of 0-0x0FFFF.

However, how can binary files larger than 64KB be linked into the project?

See more...

  • No labels