You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 4 Next »

e2 studio + Smart configrator

(1) Select [File] β†’ [New] β†’ [Renesas C/C++ Project] β†’ [Renesas RL78] to activate the project creation wizard.

​ 

(2) In the project creation wizard, select [Renesas RL78] β†’ [Renesas CC-RL C Executable Project] or [LLVM for Renesas RL78 C/C++ Executable Project], and click on the [Next] button. ​

Β 

(3) Enter project information (Give the project a name – no spaces or special characters.). Click on the [Next] button to continue.

​ 

(4) Select the toolchain, device, and debug configuration. Click on the [Next] button. (e.g. Target Device: RL78G23 – 64 pins (Part number: R7F100GLGxFB)) ​

Β 

  • No labels