If you encounter any issues after the upgrade, please open a support request TICKET.π
(1) Select [File] β [New] β [Renesas C/C++ Project] β [Renesas RL78] to activate the project creation wizard.
βΒ
(2) In the project creation wizard, select [Renesas RL78] β [Renesas CC-RL C Executable Project] or [LLVM for Renesas RL78 C/C++ Executable Project], and click on the [Next] button. β
(3) Enter project information (Give the project a name β no spaces or special characters.). Click on the [Next] button to continue.
βΒ
(4) Select the toolchain, device, and debug configuration. Click on the [Next] button. (e.g. Target Device: RL78G23 β 64 pins (Part number: R7F100GLGxFB)) β