When using iptables command on RZ/G2L series board and RZ/Five, below error occurs.
root@smarc-rzg2ul:~# iptables -L modprobe: FATAL: Module ip_tables not found in directory /lib/modules/5.10.83-cip1-yocto-standard iptables v1.8.4 (legacy): can't initialize iptables table `filter': Table does not exist (do you need to insmod?) Perhaps iptables or your kernel needs to be upgraded.
Please use below bitbake command to change the kernel configuration:
# command to open the menuconfig tool $ bitbake linux-renesas -c menuconfig
Please change enable below kernel configuration:
[*] Networking support ---> Networking options ---> [*] Network packet filtering framework (Netfilter) ---> Core Netfilter Configuration ---> <*> Netfilter connection tracking support IP: Netfilter Configuration ---> <*> IP tables support (required for filtering/masq/NAT) <*> Packet filtering <*> iptables NAT support <*> MASQUERADE target support
After the kernel configuration was fixed, please use bitbake to start the build progress.
# start the system build with bitbake command $ bitbake core-image-<minimal/bsp/weston/qt>
If the below error happened when using ip6tables command on RZ/G2L series board and RZ/Five, users can fix it by changing kernel configuration.
# error logged when using command "ip6tables" root@smarc-rzg2ul:~# ip6tables -L modprobe: FATAL: Module ip6_tables not found in directory /lib/modules/5.10.83-cip1-yocto-standard ip6tables v1.8.4 (legacy): can't initialize ip6tables table `filter': Table does not exist (do you need to insmod?) Perhaps ip6tables or your kernel needs to be upgraded.
Kernel configuration to support ip6tables.
[*] Networking support ---> Networking options ---> <*>The IPv6 protocol ---> [*] Network packet filtering framework (Netfilter) ---> IPv6: Netfilter Configuration ---> <*> IP6 tables support (required for filtering) <*> Packet filtering <*> ip6tables NAT support <*> MASQUERADE target support
When using ip command to configure the VLAN on RZ/G device, the below error message may occur.
root@smarc-rzg2ul:~# ip link add link eth0 name eth0.100 type vlan id 100 Error: Unknown device type.
Please change the kernel configuration as below and restart the build progress.
[*] Networking support ---> Networking options ---> <*> 802.1Q/802.1ad VLAN Support [*] GVRP (GARP VLAN Registration Protocol) support [*] MVRP (Multiple VLAN Registration Protocol) support
Following packages can be installed in the system to improve the functionality of networking
The bridge-utils package contains a utility needed to create and manage bridge devices on RZ/G2 boards.
A bridge is a type of software used to bind multiple network segments together. The bridge acts like a virtual network switch and works transparently (other machines don't need to know it exists). You can connect real devices (eg eth0) and virtual devices (eg tap0) to the bridge.
To install the bridge-utils package, you can add "bridge-utils" to IMAGE_INSTALL_append variable in local.conf.
# in local.conf IMAGE_INSTALL_append = " bridge-utils "
NOTE: User may need to enable both ethernet ports on an EVK. Please refer chapter "Add ipatbles support".
To enable the support of bridge function, below kernel configuration should be added with command "bitbake linux-renesas -c menuconfig".
$ bitbake linux-renesas -c menuconfig
[*] Networking support ---> Networking options ---> [*] Network packet filtering framework (Netfilter) ---> <*> Bridged IP/ARP packets filtering Core Netfilter Configuration ---> <*> Netfilter Xtables support (required for ip_tables) <*> Ethernet Bridge tables (ebtables) support ---> <*> ebt: broute table support <*> ebt: filter table support <*> ebt: nat table support <*> ebt: 802.3 filter support <*> ebt: among filter support <*> ebt: ARP filter support <*> ebt: IP filter support <*> ebt: limit match support <*> ebt: mark filter support <*> ebt: packet type filter support <*> ebt: STP filter support <*> ebt: 802.1Q VLAN filter support <*> ebt: arp reply target support <*> ebt: dnat target support <*> ebt: mark target support <*> ebt: redirect target support <*> ebt: snat target support <*> ebt: log support <*> 802.1d Ethernet Bridging
When kernel configuration is edited, issue command to enable system build.
bitbake core-image-<minimal/bsp/weston/qt>
Users can set a bridge with the command brctl on EVK.
# set a bridge br0 $ brctl addbr br0 # Add port eth0 and eth1 to bridge br0 $ brctl addif br0 eth0 eth1 # set ip address for br0 $ ifconfig br0 192.168.10.200
RP-PPPoE is a PPPoE client, relay and server for Linux. It can run completely in user-mode or used the Linux kernel's built-in PPPoE support. Here is the homepage of RP-PPPoE project.
You can enable pppoe client and server by adding the code below to local.conf:
# code to enable pppoe client and server in local.conf IMAGE_INSTALL_append = " rp-pppoe rp-pppoe-server "
To enable pppoe function, following kernel configuration must be enabled.
Device Drivers ---> [*] Network device support ---> <*> PPP (point-to-point protocol) support <*> PPP over Ethernet <*> PPP support for async serial ports <*> PPP BSD-Compress compression <*> PPP Deflate compression <*> PPP support for sync tty ports Character devices ---> [*] Non-standard serial port support <*> HDLC line discipline support
NetworkManager is a system service that manages network interfaces and connections based on user or automatic configuration. It supports Ethernet, Bridge, VLAN, Wi-Fi, PPPoE and other devices, and supports a variety of different VPN services.
NOTE: Networkmaneger packages and its dependencies require removing the restriction on GPLv3 and GPLv3+ license.
To enable networkmanager in rootfs image, please add the below code to local.conf.
# add networkmaneger IMAGE_INSTALL_append = " networkmanager " # Exclude packages for networkmanager PACKAGE_EXCLUDE = " connman connman-client connman-tests connman-tools connman-t-online " # Comment out the restriction on GPLv3 and GPLv3+ license #INCOMPATIBLE_LICENSE = "GPLv3 GPLv3+"
VLAN (Virtual LAN) is a technology that creates a virtual LAN segment independent of the physical connection form. VLANs are used to logically divide LAN segments inside the switch. By using VLAN broadcast domains can be divided with L2 switches in the same way as with routers and L3 switches.
To add vlan to rootfs image, please add below code to local.conf.
IMAGE_INSTALL_append = " vlan "
To enable routing between the different vlans, please run the below command on the evaluation board:
# Enable ip forward to enable routing between vlans $ echo 1 > /proc/sys/net/ipv4/ip_forward
tcpdump is a powerful command-line packet analyzer. It allows the user to display TCP/IP and other packets being transmitted or received over a network.
To enable this package in rootfs image, please use the below code in local.conf:
IMAGE_INSTALL_append = " tcpdump "
The following packages are for the Wifi support on RZ/G board. Packages listed in this section are required by RZ/G2L series board and RZ/Five, if user wants the corresponding Wifi support. For RZ/G2 series board, these packages are not necessary due to they already have Wifi enabled by default.
On RZ/G2L series board, user will need WiFi adapter the WiFi adapter used by us is BUFFALO WLI-UC-G301N. Wifi adapters requires support from kernel. Please enable the below kernel configuration.
Device Drivers ---> [*] Network device support ---> <*> USB Network Adapters ---> <*> Multi-purpose USB Networking Framework
Device Drivers ---> [*] USB support ---> <*> USB Wireless Device Management support
Please set the wireless configuration as below:
Networking support ---> [*] Wireless ---> <*> cfg80211 - wireless configuration API [*] nl80211 testmode command [*] enable developer warnings [*] enable powersave by default (NEW) [*] cfg80211 DebugFS entries [*] cfg80211 wireless extensions compatibility <*> Generic IEEE 802.11 Networking Stack (mac80211) Default rate control algorithm (Minstrel) ---> [*] Enable mac80211 mesh networking support [*] Enable LED triggers [*] Export mac80211 internals in DebugFS [*] Trace all mac80211 debug messages [*] Select mac80211 debugging features --->
This is the Central Regulatory Domain Agent for Linux. It serves one purpose: tell Linux kernel what regulatory rules to enforce for 802.11. CRDA searches for available frequency bands in the regulatory information database provided by the wireless-regdb package.
When using Wifi adapter from TP-Link without this package, user will see kernel message:
cfg80211: failed to load regulatory.db
Please add this package with the code below to remove the above error message:
IMAGE_INSTALL_append = " crda "
hostapd (host access point daemon) is a user space daemon software enabling a network interface card to act as an access point and authentication server.
Let RZ/G board be a Wifi access point. Please add the code in local.conf:
IMAGE_INSTALL_append = " hostapd "
Please add settings for adapter to hostapd file /etc/hostapd.conf
# in file /etc/hostapd.conf interface=wlan0 driver=nl80211 ssid=<Wifi SSID> hw_mode=g channel=1 wmm_enabled=1 macaddr_acl=0 auth_algs=1 wpa=2 wpa_key_mgmt=WPA-PSK rsn_pairwise=CCMP wpa_passphrase=<Wifi password>
To check the setting in file /etc/hostapd.conf, please use the below command. There should be no error message if the setting was correct.
# Check settings in file /etc/hostapd.conf $ hostapd -dd /etc/hostapd.conf
Users can start/stop hostapd manually with the below command:
# Start the hostapd service $ systemctl start hostapd # Stop the hostapd service $ systemctl stop hostapd
To offer support for 802.11 standard WLAN settings, iw package is provided as wireless tool and can be installed with the code below in local.conf:
IMAGE_INSTALL_append = " iw "
linux-firmware is a package distributed together with the Linux kernel that contains the firmware binary blobs necessary for the functioning of a particular hardware device.
Use below code to add this package:
IMAGE_INSTALL_append = " linux-firmware "
wpa_supplicant is a cross-platform supplicant that supports WEP, WPA, WPA2 (IEEE 802.11i / RSN (Robust Secure Network)). It targets desktops, laptops and embedded systems.
Please add this package with below code:
IMAGE_INSTALL_append = " wpa-supplicant "
Packages for supporting the bluetooth function on RZ/G board. We have tested with bluetooth adapter TP-Link UB500 Bluetooth 5.0.
bluez5: bluetooth protocol stack for Linux system.
Add bluez5 package with code:
IMAGE_INSTALL_append = " bluez5 "
Bluetooth support requires changing configurations as below:
Networking support ---> Bluetooth subsystem support ---> [*] Bluetooth Classic (BR/EDR) features (NEW) <*> RFCOMM protocol support [ ] RFCOMM TTY support (NEW) < > BNEP protocol support (NEW) <*> HIDP protocol support [*] Bluetooth High Speed (HS) features [*] Bluetooth Low Energy (LE) features (NEW) [ ] Enable LED triggers (NEW) [ ] Enable Microsoft extensions (NEW) [*] Export Bluetooth internals in debugfs (NEW) [ ] Bluetooth self testing support (NEW) [ ] Enable runtime option for debugging statements (NEW) Bluetooth device drivers --->
bluez5 will install bluetoothctl command to system. Bluetooth pairing and connect with this command will be as below:
# Start bluetoothctl root@smarc-rzfive:~# bluetoothctl Agent registered [CHG] Controller E8:48:B8:C8:20:00 Pairable: yes [bluetooth]# power on Changing power on succeeded [CHG] Controller E8:48:B8:C8:20:00 Powered: yes # Scan bluetooth devices [bluetooth]# devices Device 10:30:25:EB:6B:xx <Deivce 1> Device 10:30:25:F1:28:yy <Device 2> Device E4:70:B8:FD:1C:zz <Device 3> Device <Device Mac> <Deivce name> # Pair device with device Mac [bluetooth]# pair 10:30:25:EB:6B:xx Attempting to pair with 10:30:25:EB:6B:xx [CHG] Device 10:30:25:EB:6B:xx Connected: yes Request confirmation [agent] Confirm passkey 028937 (yes/no): yes [CHG] Device 10:30:25:EB:6B:xx Connected: no [CHG] Device 10:30:25:EB:6B:xx Paired: yes Pairing successful [bluetooth]#
Below an example to check the basic CAN functionality in Linux. It refers to RZ/G2L but it should work as is also for RZ/G2LC-UL and RZ/V2L.
devmem2 is used to configure the relevant registers.
Enable Global test mode (GMDC[1:0]=0x2) in the Global Control Register:
root@smarc-rzg2l:~# devmem2 0x10050088 w 0xA02 /dev/mem opened. Memory mapped at address 0xffff8f046000. Read at address 0x10050088 (0xffff8f046088): 0x00000A00 Write at address 0x10050088 (0xffff8f046088): 0x00000A02, readback 0x00000A02
Enable Inter-Channel Communication Test (CnICBCE = 1) in the Global Test Configuration Register:
root@smarc-rzg2l:~# devmem2 0x10050468 w 0x3 /dev/mem opened. Memory mapped at address 0xffffb60af000. Read at address 0x10050468 (0xffffb60af468): 0x00000000 Write at address 0x10050468 (0xffffb60af468): 0x00000003, readback 0x00000003
Enable Communication Test between Channels (ICBCTME=1) in the Global Test Control Register:
root@smarc-rzg2l:~# devmem2 0x1005046C w 0x1 /dev/mem opened. Memory mapped at address 0xffff9f827000. Read at address 0x1005046C (0xffff9f82746c): 0x00000000 Write at address 0x1005046C (0xffff9f82746c): 0x00000001, readback 0x00000001
Configure can0 and can1 (FD enabled):
root@smarc-rzg2l:~# ip link set can0 type can bitrate 333333 dbitrate 666666 fd on root@smarc-rzg2l:~# ip link set can1 type can bitrate 333333 dbitrate 666666 fd on
Disable Global test mode (GMDC[1:0]=0x0) in the Global Control Register:
root@smarc-rzg2l:~# devmem2 0x10050088 w 0xA00 /dev/mem opened. Memory mapped at address 0xffff9cab3000. Read at address 0x10050088 (0xffff9cab3088): 0x00000A02 Write at address 0x10050088 (0xffff9cab3088): 0x00000A00, readback 0x00000A00
can0 and can1 link up:
root@smarc-rzg2l:~# ip link set can1 up root@smarc-rzg2l:~# ip link set can0 up
Start candump for can0 and can1 to log any can communication:
root@smarc-rzg2l:~# candump can0 & candump can1 & [1] 292 [2] 293
Send a sample CAN message using can1:
root@smarc-rzg2l:~# cansend can1 18ff6228#aa55aa55aa55aa55 can1 18FF6228 [8] AA 55 AA 55 AA 55 AA 55 can0 18FF6228 [8] AA 55 AA 55 AA 55 AA 55
As expected the message is captured by both CAN interfaces.
If you want to send CAN-FD frames just use two "#" followed by a "0" (no increase in bitrate) or "1" (switch to higher bitrate). E.g.
root@smarc-rzg2l:~# cansend can1 18ff6228##1aa55aa55aa55aa55aa55aa55aa55aa55aa55aa55aa55aa55aa55aa55aa55aa55 can1 18FF6228 [32] AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 can0 18FF6228 [32] AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55 AA 55
Note: obviously this test works only if the CAN transceiver is fitted. Many EVKs shipped recently do not have the transceiver populated. First check that IC15 is soldered on the board.
Configure can1 and set up link (as previous section):
root@smarc-rzg2l:~# ip link set can1 type can bitrate 333333 dbitrate 666666 fd on root@smarc-rzg2l:~# ip link set can1 up
Halt can1 CHMDC[1:0]=0x2 in the Channel 1 Control register:
devmem2 0x10050014 w 0x00A1FF02
Configure self-test mode 0 (external loopback mode) by setting CTMS[1:0]=0x2 as well as CTME=1 in the Channel 1 Control register and set can1 back to Channel communication mode (CHMDC[1:0]=0x0):
devmem2 0x10050014 w 0x05A1FF00
Then candump and cansend similar to previous example:
candump can1 & cansend can1 18ff6228#55aa55aa55aa55aa can1 18FF6228 [8] 55 AA 55 AA 55 AA 55 AA can1 18FF6228 [8] 55 AA 55 AA 55 AA 55 AA
Exactly same as External loopback test, the only difference is the CTMS[1:0] configuration (0x3):
devmem2 0x10050014 w 0x07A1FF00