You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 2 Next »

RZ/A Series 32-bit MPU

Introduction

This page is for the Renesas RZ/A family of embedded SoCs. The main goal is to make the information about RZ/A SoCs friendly, easy to access for embedded developers.

The links below can be used to get familiar with Renesas RZ/A SoC


Boards

  • Here is the list of available Renesas Evaluation Boards (bottom of page).
  • The board pages below contain instructions for downloading and building the BSP as well as other useful information about the boards.

RZ/A3


 RZA3UL Evaluation board

RZA3UL
by Renesas

RZ/A2M


 RZA2M Evaluation board

RZA2M
by Renesas

 RZA2M MBED Mango

[1]
by Renesas MBED

RZ/A1


 Stream It kit

RZ/A1LU
by Renesas
 RZ/A1H Starter Kit

RZA/1H
by Renesas

 GR-LYCHEE

[2]RZ/A1LU
by Renesas MBED

 GR-PEACH

[3]RZ/A1H
by Renesas MBED

Official Software and Documentation

These are the currently supported Software packages for the RZA1 and RZA2M. The

Renesas Supported Development Environments

  • Renesas e2studio
  • RZA1 Smart Configurator
    • NOTE: The RZA1 is not supported on the Smart Configurator found in the Renesas e2studio IDE.
    • This Smart Conjugator is a standalone application
    • Hardware Pin Configuration is supported
    • Code Generation not supported

RZA GUI Platforms

RZA Bootloaders

Below are links to Source code for the RZ/A bootloaders and firmware update. These are reference code that was designed for the Renesas RZ/A EVKs. Included below are links to porting documentation.

RZA1

  • RZ/A1 Bootloader
    • RZ/A1H Group Example of Booting from Serial Flash Memory doc and Source Code
    • RZ/A1LU QSPI Flash Boot Loader doc and Source Code
    • RZ/A1LU Group Example of Booting from Serial Flash Memory doc and Source Code
  • RZA firmware update
    • The RZA1 does not have Firmware Update reference code.
    • Refer to the RZA2M Firmware Update for Serial Flash Driver to port to the RZA1.

RZA2M

Articles and Whitepapers

Topics

FAQ

  • No labels