You are viewing an old version of this page. View the current version.
Compare with Current View Page History
« Previous Version 4 Next »
Target Ubuntu OS Version: 20.04, 18.04
Target reference board: RZ/G2L,/G2LC,/G2UL SMARC
Host PC Environment: Ubuntu20.04
Run below command on Host Ubuntu PC
sudo apt-get install qemu-user-static
wget https://cdimage.ubuntu.com/ubuntu-base/releases/20.04/release/ubuntu-base-20.04.4-base-arm64.tar.gz or wget https://cdimage.ubuntu.com/ubuntu-base/releases/focal/release/ubuntu-base-20.04.4-base-arm64.tar.gz
wget http://cdimage.ubuntu.com/ubuntubase/releases/18.04.5/release/ubuntu-base-18.04.5-basearm64.tar.gz |
In the following example, please replace "version" as below name as you need
ubuntu-base-20.04.4-base-arm64: 20.04.4
ubuntu-base-18.04.5-base-arm64: 18.04.5
mkdir root
sudo tar -xpf ubuntu-base-<version>-base-arm64.tar.gz -C root
sudo cp /usr/bin/qemu-aarch64-static ./root/usr/bin/
sudo cp -b /etc/resolv.conf root/etc/resolv.conf
vim ch-mount.sh#!/bin/bash function mnt() { echo "MOUNTING" sudo mount -t proc /proc ${2}proc sudo mount -t sysfs /sys ${2}sys sudo mount -o bind /dev ${2}dev sudo chroot ${2} } function umnt() { echo "UNMOUNTING" sudo umount ${2}proc sudo umount ${2}sys sudo umount ${2}dev } if [ "$1" == "-m" ] && [ -n "$2" ] ; then mnt $1 $2 elif [ "$1" == "-u" ] && [ -n "$2" ]; then umnt $1 $2 else echo "" echo "Either 1'st, 2'nd or both parameters were missing" echo "" echo "1'st parameter can be one of these: -m(mount) OR -u(umount)" echo "2'nd parameter is the full path of rootfs directory(with trailing '/')" echo "" echo "For example: ch-mount -m /media/sdcard/" echo "" echo 1st parameter : ${1} echo 2nd parameter : ${2} fi |
chmod +x ch-mount.sh ./ch-mount.sh -m root/ chmod -R 777 /tmp
apt-get update
apt-get install \ language-pack-en-base \ sudo \ ssh \ net-tools \ network-manager \ ethtool \ ifupdown \ isc-dhcp-client \ openssh-server \ iputils-ping \ rsyslog \ bash-completion \ htop \ resolvconf \ dialog \ vim
useradd -s '/bin/bash' -m -G adm,sudo <name>
passwd <name>
passwd root
chown -R root:root /bin/su
chmod u+s /bin/su
start on stopped rc or RUNLEVEL=[12345]
stop on RUNLEVEL [!12345]
respawn exec /sbin/getty -L 115200 ttyLP0 vt102
echo "auto eth0" > /etc/network/interfaces.d/eth0 echo "iface eth0 inet dhcp" >> /etc/network/interfaces.d/eth0 echo "nameserver 8.8.8.8" >> /etc/resolv.conf echo "nameserver 8.8.4.4" >> /etc/resolv.conf
exit ./ch-mount.sh -u root/
cd root tar -cjf rootfs.tar.bz2 ./*
Prepare a SD card with ext4 partition: SD Card Loading and Booting
extract ubuntu rootfs package to SD card
sudo tar -xvf rootfs.tar.gz -C /media/xxx/rootfs
Copy the Wayland 1.18.0 source code from VLP Yocto build folder to SD card home folder.
i.e. build/tmp/work/aarch64-poky-linux/wayland/1.18.0-r0/wayland-1.18.0/
Copy the wayland-protocol1.20.0 source code from VLP Yocto build folder to SD card home folder.
i.e. build/tmp/work/aarch64-poky-linux/wayland-protocols/1.20-r0/wayland-protocols-1.20/
Copy the weston8.0.0 source code from VLP Yocto build folder to SD card home folder.
i.e. build/tmp/work/aarch64-poky-linux/weston/8.0.0-r0/weston-8.0.0/
|
If the configuration is correct, it will display below messages
User defined options libdir : /usr/lib/aarch64-linux-gnu prefix : /usr sysconfdir : /etc backend-drm-screencast-vaapi : false color-management-colord : false remoting : false xwayland : false
Please refer to the StartupGuide.txt document in meta-rz-features/recipes-graphics/mali/files/mali_pkg_eval_vx.x.tar.gz
Copy the driver mali_kbase..ko from VLP Yocto build folder to SD card.
i.e. build/tmp/work/smarc_rzg2l-poky-linux/kernel-modulemali/r35-p0/image/lib/modules/5.10.83-cip1-yocto-standard/extra
|
Copy the library files to SD card.
i.e. meta-rz-features/recipesgraphics/mali/files/mali_pkg_eval_vx.x.tar.gz
Expandinstall library to reference board |
/usr/lib/aarch64-linux-gnu/
sudo apt install glmark2-es2-wayland
Only root user can launch weston service, please switch to root user in advance
insmod mali_kbase.ko
export XDG_RUNTIME_DIR=/usr/lib/ export RUNLEVEL=3
weston --tty 1 &
Run glmark2 test
glmark2-es2-wayland --fullscreen
In this section, we will copy codec related files from original VLP Yocto build.
i.e. core-image-qt-smarc-rzg2l.tar.bz2 or core-image-weston-smarc-rzg2l.tar.bz2
Pleaes copy this .bz2 file to Ubuntu SD card and run below instruction on reference board
unzip core-image-qt-smarc-rzg2l.tar.bz2 or core-image-weston-smarc-rzg2l.tar.bz2 to folder "yocto"
copy codec drivers |
|
copy gstreamer related lib |
|
modify omx plugin configuration |
vi /etc/xdg/gstomx.conf replace "lib64" as "lib/aarch64-linux-gnu" [omxh264dec] type-name=GstOMXH264Dec core-name=/usr/lib/aarch64-linux-gnu/libomxr_core.so component-name=OMX.RENESAS.VIDEO.DECODER.H264 ····· [omxh264enc] type-name=GstOMXH264Enc core-name=/usr/lib/aarch64-linux-gnu/libomxr_core.so component-name=OMX.RENESAS.VIDEO.ENCODER.H264 ···· |
install gstreamer dependency |
apt install gstreamer1.0-libav gstreamer1.0-plugins-bad |
login as root and insmod drivers |
insmod /root/modules/mali_kbase.ko insmod /root/modules/mmngr.ko insmod /root/modules/mmngrbuf.ko insmod /root/modules/uvcs_drv.ko insmod /root/modules/vspm.ko insmod /root/modules/vspm_if.ko |
Specify gstreamer location |
export GST_PLUGIN_SCANNER=/usr/lib/aarch64-linux-gnu/gstreamer-1.0/gst-plugin-scanner export GST_PLUGIN_PATH=/usr/lib/aarch64-linux-gnu/gstreamer-1.0 |
Launch weston |
weston –tty 1 & |
Play Video |
gst-launch-1.0 filesrc location=/root/video/sintel_trailer-720p.mp4 ! qtdemux ! queue ! h264parse ! omxh264dec ! waylandsink
gst-launch-1.0 filesrc location=/root/video/sintel_trailer-720p.mp4 ! qtdemux name=d d. ! queue ! h264parse ! omxh264dec ! waylandsink d. ! queue ! faad ! alsasink device=plughw:0,0 |
You can port Qt by following 3 methods
In this section, we will copy Qt5.6.3 related files from original VLP Yocto build.
i.e. core-image-qt-smarc-rzg2l.tar.bz2
Pleaes copy this .bz2 file to Ubuntu SD card and run below instruction on reference board
unzip core-image-qt-smarc-rzg2l.tar.bz2 to folder "yocto"
(For other version of Qt, you can modify Yocto meta-qt5\recipes-qt\qt5, please inqury Qt company for higher version QT integration)
Port Qt lib |
cd yocto cp -rd usr/share/qt5 /usr/share/ cp -rd usr/lib64/qt5 /usr/lib/aarch64-linux-gnu/ cp -rd usr/lib64/libQt* /usr/lib/aarch64-linux-gnu/ cp -rd usr/lib64/pkgconfig/Qt* /usr/lib/aarch64-linuxgnu/pkgconfig/ export QT_QPA_PLATFORM=wayland export QT_PLUGIN_PATH=/usr/lib/aarch64-linux-gnu/qt5/plugins/ |
Start Weston RZ-G/RZ-G2 BSP Porting Ubuntu#Start Weston desktop
Then run the Qt example in /usr/share/qt5/examples
You can download qt5 source to reference board and compile on board.
Or cross compile qt5 on PC
Or compile qt5 in PC QEMU
Here we compile qt5 on board
Collapsecompile qt5 |
download qt5 source code by git (ignore) mkdir qt5-build cd qt5-build make make install (rsync to SD) |
We suggest to compile the qt5 with scrips
Notes: About the flags parameter in configure of Qt5. -qpa should be set as wayland or wayland-egl. We didn't support xcomposite-egl option
apt-get install qt5-default qtwayland5
Notes: The above installation commands can only run part of Qt functions. If you need more functions, you need to continue installing Qt related packages.
This section introduce how to develop Qt application on PC.
bitbake core-image-qt -c populate_sdk
The generated installation file is located at:
build/tmp/deploy/sdk/poky-glibc-x86_64-core-image-qtaarch64-smarc-rzg2l-toolchain-3.1.14.sh
Install this SDK to PC, default folder is /opt/poky/3.1.14
setup SDK runtime environment
source /opt/poky/3.1.14/environment-setup-aarch64-poky-linux
Add Device | |
---|---|
Add new Kit | |
Add Qt version | |
Add compiler | |
Add debuggers | |
Select kit to build Qt project | |
example to run qt calculator project |