RZ/G3S
Getting Started
📄 Easy download guide
- The easy download guide can be found on renesas.com.
- This document regroups all links necessary for the user to develop an application.
📦 What is included in the Box
- RZ/G3S SMARC Module board
- RZ SMARC Series Carrier Board II
- RZ SMARC Series JTAG adaptor cable
- USB Type-A to USB Micro B cable for serial debug
- Accessories: Screws and spacer
🛒 What you will need to purchase
- Power: (Required) USB Type-C power supply.
⭐ Pre-Built Binaries ⭐
- If you prefer to program pre-built binaries into your board, you can find the link to download them in easy download guide from renesas.com
- The package includes a complete SD Card image that can be written using Windows or Linux.
- Boot loaders are also included in the package.
- On the downloaded Pre-built Image package, you can find Pre-built images guide. Please follow the instruction in the guide to program the prebuilt image.
💻 Build Environment
- To build the BSP, you will need a Linux PC running Ubuntu 20.04. This was the only host OS that was tested, and that specific version is a requirement of Yocto 3.1 (dunfell). Using Ubuntu 22.04 will not work.
- You can use a Linux PC (recommended) or a Virtual Machine. If using a Virtual Machine, 200GB of hard drive space is recommended for the minimum build.
- If you are not currently running Ubuntu 20.04, you can use a docker container.
- Example: Host Machine = Ubuntu 22.04 + Docker Container running Ubuntu 20.04 inside of it.
- Some setup instructions and scripts are provided to make it easy to get started.
💾 Downloading the Linux BSP
- Download the RZ/G2L Board Support Package from renesas.com
🔨 Building the BSP
- Build Instructions: The instructions for building the BSP are located in the Release Note document that is included in the ZIP file download from renesas.com.
⚡ Programing the Board