This is a sumary of how to run a TVM model on the RZV board. The code snippest are based on the TVM Tutorial Application that can be foundΒ here.Β The TMV Runtime Inference API is part of the EdgeCortix MERA software. The API for the EdgeCortix MERA softwre is defined in the header fileΒ MeraDrpRuntimeWrapper.h. The DRP-AI pre-processing is defined in the TVM Applicaton Document appendixΒ hereΒ .
It is requred that TVM applications be deployed as follows.
/ βββ usr β βββ lib64 β βββ libtvm_runtime.so βββ home βββ root βββ tvm βββ preprocess_tvm_v2ma β βββ drp_param.bin β ... β βββ preprocess_tvm_v2ma_weight.dat βββ resnet18_onnx β βββ deploy.json β βββ deploy.params β βββ deploy.so βββ sample.yuv βββ synset_words_imagenet.txt βββ tutorial_app
Step 1)Β LoadΒ pre_dirΒ object to DRP-AI. The pre-processing object directoryΒ pre_dirΒ contains the Renesas pre-compiled files located in the ${TVM_ROOT}/apps/exe/preprocess_tvm_<v2xx> (v2l, v2m, v2ma).
preruntime.Load(pre_dir);
Step 2)Β Load TVM Translated inference model directory and its weight from theΒ model_dirΒ to runtime object.
runtime.LoadModel(model_dir);
Step 3)Β Allocate continuous memory for the Camera capture buffer. Pre-processing Runtime requires the input buffer to be allocated in contiguous memory area. This application uses imagebuf (u-dma-buf) contiguous memory area. Refer for this page about the Linux Contiguous Memory AreaΒ here.
This section describes the steps to run the TVM AI model. It is recommended that this section and the Post-processing section run in a thread.Β In-addition the Camera Capture should also be run in a separate thread.
Step 1)Β Read camera image. Refer to TVM code example.Β Step 2)Β Set Pre-processing parameters and run the pre-processing model. The DRP Pre-processing operations are format conversion ( YUV422 to RGB ), Resize, and input normalization.
preproc_param_t in_param; in_param.pre_in_addr = udmabuf_addr_start; in_param.pre_in_shape_w = INPUT_IMAGE_W; in_param.pre_in_shape_h = INPUT_IMAGE_H; in_param.pre_in_format = INPUT_YUYV; in_param.resize_w = MODEL_IN_W; in_param.resize_h = MODEL_IN_H; in_param.resize_alg = ALG_BILINEAR; /*Compute normalize coefficient, cof_add/cof_mul for DRP-AI from mean/std */ in_param.cof_add[0]= -255*mean[0]; in_param.cof_add[1]= -255*mean[1]; in_param.cof_add[2]= -255*mean[2]; in_param.cof_mul[0]= 1/(std[0]*255); in_param.cof_mul[1]= 1/(std[1]*255); in_param.cof_mul[2]= 1/(std[2]*255); ret = preruntime.Pre(&in_param, &output_ptr, &out_size);
Step 3)Β Set Pre-processing output to be inference input.
runtime.SetInput(0, output_ptr);
Step 4)Β Run Inference. This is a synchrous function call that waits on the completion of the TVM Runtime. I
runtime.Run();
Becasse TVM off loadsΒ operation to the CPU the **final** output datatype could be Floating point 32 (FP32) or Floating point 16 (FP16). The FP32 is the final output from the CPU. The FP16 datatype is the final ouput from the DRP.
Step 1)Β Read data from DRP memory to an array. This is informaiton is done as follows:
/* Comparing output with reference.*/ /* output_buffer below is tuple, which is { data type, address of output data, number of elements } */ auto output_buffer = runtime.GetOutput(0); int64_t out_size = std::get<2>(output_buffer); /* Array to store the FP32 output data from inference. */ float floatarr[out_size];
datatype == FP16
if (InOutDataType::FLOAT16 == std::get<0>(output_buffer)) { /* Read the dataout and convert to FP32 */ }
datatype == FP32
if (InOutDataType::FLOAT32 == std::get<0>(output_buffer)) { /* Just Read to memory */ }
Step 2)Β Parse the output for Classification and/or Boundary box The output depends on the AI model used. The TVM Demo **tutorial_app** demonstrates the RESNET Model. The output of this classification models is an array of 1000 classification. Simple fined the highest confidense value of the array. Last check if max confidense value is above a defined threshold.