Overview
This page focuses on detailed topics specific to RL78. Here, you will find discussions on new peripherals, software, hardware, tools, and technologies related to RL78, Code Generator, and Smart Configurator. We also share how-to guides and our experiences to assist you with your designs.
RL78 Specific Topics
Below are several specific topics designed to support your development, many of which stem from real-world challenges we helped customers address. These topics delve deeper into the details and may include custom documentation we created to highlight issues and their solutions.
Worried about OTA Failure Bricking Your Device? Boot Swap Can Help You
This section mainly explains how to use the existing program to update the firmware in the flash. Using this method, the code flash is divided into two areas: the execution area and the temporary area. The Renesas Flash Driver RL78RFD Type02 is used to reprogram the flash and perform boot swapping. This explanation mainly takes RL78/F24 as an example to explain how to implement boot swapping.
Worried about OTA failure bricking your device? Boot swap can help you
Using LIN Module (RLIN3) with Software Integration System (SIS)
This topic is applicable to RL78/F24. The LIN/UART module (RLIN3) is a hardware LIN communication controller that supports LIN Specification Package Revision 1.3, 2.0, 2.1, 2.2 and SAE J2602, and automatically performs frame communication and error determination. You can find out more information how to get started with RLIN3 and using the Renesas LIN Configurator.
Getting Started with LIN for RL78/F2x MCU's