the GSE is backwards compatible, so it can always load projects from versions 2.0 and later. But this might have limitations when dealing with custom-extensions. These need to be known by the GSE or else it will have problems loading the file. In this case the problem exists in the file MainDlg.xml in the line 19299. You could check the file if the control which should be loaded is a CustomExtension and then check if the customextension is registered in the GSE. To do this just scroll down the Control-Catalog and check if the CustomExtension is available. If the CustomExtension is in the list this problem might have some other reason. You can do another check by activating the setting "skip corrupted data in dialogs..." in the Settings-dialog. This will output more information about the problem when loading the project again. But please be aware that the GSE will now drop controls which can not be loaded resulting in a modified project where these controls have been removed. So it is advised to check this on a copy of the project.
SR_GuilianiDemo on RZA2M but it throws following error while debugging. Error - "Can't find a source file at "C:/JenkinsSlave/workspace/Renesas/Guiliani_SDK_2.3_Renesas_RZA2M_FreeRTOS10_eGML/Guiliani/Source/Core/GUIResourceFileHandler.cpp" Can't find a source file at "C:/JenkinsSlave/workspace/Renesas/Guiliani_SDK_2.3_Renesas_RZA2M_FreeRTOS10_eGML/Guiliani/Source/Core/GUIResourceFileHandler.cpp"
The TES Guiliani application fails with random exceptions after hours of operation.
Diagnosis indicates FPU register corruption during context switches.
The root cause is likely that FreeRTOS is not properly saving/restoring FPU/NEON registers when switching tasks.
FreeRTOS Configuration for FPU/NEON Support
By default, FreeRTOS does not automatically save FPU/NEON registers unless explicitly configured.
The setting configUSE_TASK_FPU_SUPPORT
controls this behavior:
0
(Default) → No FPU context saving (risks corruption if tasks use FPU).
1
→ Lazy stacking (only saves FPU registers if a task uses them, but may not cover NEON).
2
→ Full FPU save/restore (always saves FPU registers on context switch.
Recommended Fix
Step 1: Set configUSE_TASK_FPU_SUPPORT = 2
in FreeRTOS.h
(ensures FPU registers are saved).