Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

Image Modified


Application Note by Renesas

This User's Manual (Application Note) explains GStreamer and the custom plug-ins created by Renesas.

Usage examples are also included.

Sample Code by Renesas

Sample code for using GStreamer on Renesas RZ devices are stored in github.

Examples for RZ/G2L-V2L

For most common use cases, refer to the gstreamer user's manual linked above. Below are reported other specific cases not covered in that document.

USB Camera Examples

Encode an .264 stream from camera (using omxh264enc)

gst-launch-1.0 v4l2src device=/dev/video0 num-buffers=300 ! video/x-raw,width=1280,height=960 ! vspmfilter dmabuf-use=true ! video/x-raw,format=NV12 ! omxh264enc control-rate=2 target-bitrate=10485760 interval_intraframes=14 periodicty-idr=2 ! video/x-h264,profile=\(string\)high,level=\(string\)4.2 ! filesink location=output_xsga.264

Stream H.264 video via Ethernet

Create .sdp file for VLC to receive stream using rtsp

Let create a file named test.sdp and copy the below content in the file
NOTE: The IP address is the IP4 is the IP address of the stream sender
m=video 9001 RTP/AVP 96, 9001 is the port number which needs to be matched with the sender port

v=0
i=RZ Board Demo
c=IN IP4 192.168.86.57
s=ESP H264 STREAM
m=video 9001 RTP/AVP 96
a=rtpmap:96 H264/90000

Save the file and launch the VLC application by clicking test.sdp file to receive the stream.

Stream H.264 compressed test-pattern video via Ethernet to VLC media player

NOTE: host ip address is the ip address of PC running VLC application
gst-launch-1.0 -v videotestsrc ! queue ! videoconvert ! queue ! video/x-raw, width=320, height=240 ! queue ! omxh264enc ! queue ! rtph264pay ! queue ! udpsink host= 192.168.86.36 port=9001

Send h.264 compressed Camera video over Ethernet to the VLC media player

gst-launch-1.0 --gst-debug=3 v4l2src device=/dev/video1 ! video/x-raw, width=1280, height=720 ! videoconvert \
! video/x-raw, format=NV12 ! omxh264enc control-rate=2 target-bitrate=10485760 interval_intraframes=14 periodicty-idr=2 use-dmabuf=false \
! video/x-h264, profile=\(string\)high,level=\(string\)4.2 ! h264parse ! rtph264pay ! queue ! udpsink host=192.168.86.36 port=9001

Send h.264 compressed MP4 video over Ethernet to the VLC media player

 gst-launch-1.0 -v filesrc location=sintel_trailer-1080p.mp4 ! decodebin ! omxh264enc ! rtph264pay ! udpsink host=192.168.86.36 port=9001

RZ GStreamer C Level API Demos

Here is a an example of how to use the GStreamer C Code API for the RZV and RZG. The demo utilizes the RZ H.264 and VSPM library.

RZ GStreamer Demo

Examples for RZ/G2UL

Compared to the big brothers the RZ/G2UL does not feature a GPU nor a HW video encoder / decoder. Nevertheless gstreamer can still be used, mainly using SW plugins and the CPU and, of course, the performance is limited due to this.

Camera

MIPI Camera Setup (OV5645 camera)

Since many VLP releases now, v412-init.sh is installed by default on the /home/root folder. It has to be run before the following commands can be given.

MIPI Camera Examples

Capture from camera and display

gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,format=ARGB,width=1280,height=960 ! vspmfilter outbuf-alloc=true ! waylandsink

Capture and Scaling and Conversion using vspmfilter

gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,format=ARGB,width=1280,height=960 ! vspmfilter outbuf-alloc=true ! video/x-raw, format=BGRA, width=640, height=480 ! waylandsink

Video decoding

As mentioned there's no HW video decoder, so SW decoding gstreamer plugins have to be used. Low resolution videos are normally played ok, medium / high resolution may be challenging.

VP8 decoding

gst-launch-1.0 filesrc location=./[VP8 encoded file].webm ! matroskademux ! avdec_vp8 ! videoconvert ! waylandsink

VP9 decoding

gst-launch-1.0 filesrc location=./[VP9 encoded file].webm ! matroskademux ! avdec_vp9 ! videoconvert ! waylandsink

H.264 decoding

gst-launch-1.0 filesrc location=./[H.264 encoded file].mp4 ! qtdemux ! h264parse ! avdec_h264 ! videoconvert ! waylandsink

H.264 decoding and down scaling

gst-launch-1.0 filesrc location=./[H.264 encoded file].mp4 ! qtdemux ! h264parse ! avdec_h264 ! videoscale ! videoconvert ! video/x-raw, width=640, height=480 ! waylandsink

Table of Contents